• Home
  • QUESTIONS & ANSWERS
  • Integrated Circuits (ICs)
  • What are the pin functions of the Motorola MC68HC908GP32?

    * Question

    What are the pin functions of the Motorola MC68HC908GP32?

    * Answer

    The Motorola MC68HC908GP32 is a 8-bit microcontroller from the HC08 family, widely used in embedded systems and automotive applications. It features several functions that allow it to interface with various peripherals and systems. Below is a summary of the pin functions of the MC68HC908GP32:

    General Pin Functionality Overview:
    The MC68HC908GP32 is housed in a 32-pin package (typically in a 32-PLCC or similar), with each pin providing specific functions depending on the configuration. Many of the pins can have multiplexed functions, meaning they can serve different purposes depending on the mode of operation or configuration of the microcontroller.

    Key Pin Functions:
    Power Supply:

    VDD: Power supply pin (typically 5V).
    VSS: Ground pin (0V).
    Clock and Reset:

    XTAL1 / CLKIN: External crystal or clock input pin for the system clock (if using an external oscillator).
    XTAL2 / CLKOUT: Output of the clock signal, used to connect to external devices or as a system clock source.
    RESET: External reset pin to initialize the microcontroller. It requires a low signal to reset the device.
    Input/Output Ports (I/O Pins): The microcontroller has multiple general-purpose I/O pins used for digital input/output operations. These pins are multiplexed and can serve several functions depending on the configuration:

    PORTA (PA0 to PA7): 8-bit I/O port.
    PORTB (PB0 to PB7): 8-bit I/O port.
    PORTC (PC0 to PC3): 4-bit I/O port (some models have a subset of pins active).
    PORTD (PD0 to PD7): In some versions of the MC68HC908GP32, this port is available as an additional I/O port.
    Special Function Pins:

    TXD: Transmit data for serial communication (USART).
    RXD: Receive data for serial communication (USART).
    SCK: Serial clock used in synchronous communication modes.
    MISO: Master-In Slave-Out for SPI communication.
    MOSI: Master-Out Slave-In for SPI communication.
    SS: Slave Select for SPI communication.
    Timers and PWM:

    TMR0 to TMR3: Timer channels for generating time delays, pulse-width modulation (PWM), and event counting. Some pins can be configured for PWM or timer functions.
    PWM: Pin(s) dedicated to Pulse Width Modulation output, used for motor control, signal generation, and similar tasks.
    Analog Functions:

    ADC: Several pins are configured as analog-to-digital converter (ADC) channels. These are used for reading analog signals and converting them to digital values.
    VREFH / VREFL: Voltage reference pins for the ADC (high and low).
    Interrupts:

    IRQ: Interrupt request pin used for external interrupt handling.
    On-Chip Programming and Debugging:

    BKGD: Background debug mode pin used for programming or debugging the microcontroller. This pin is used in conjunction with the on-chip background debug interface (BDM).
    Additional Pins:

    AD0 to AD7: Analog-to-digital converter (ADC) input channels for sampling analog signals.
    VSTBY: Standby pin, used in low-power modes to control the microcontroller’s power state.
    SDA / SCL: For I2C (Inter-Integrated Circuit) communication in some configurations.

    Conclusion:
    The Motorola MC68HC908GP32 microcontroller offers a variety of pins for different functions like general I/O, serial communication (USART, SPI), analog-to-digital conversion (ADC), PWM generation, and more. The exact pin functions may depend on the specific microcontroller configuration, but in general, it provides a versatile set of interfaces for embedded system development.