• Home
  • QUESTIONS & ANSWERS
  • Power Supplies - Board Mount
  • What are the pin functions of the TPS6205×?

    * Question

    What are the pin functions of the TPS6205×?


    *
    Answer

    EN: Enable, when it is low, it is off.FB: Feedback pin for fixed voltage output.GND, PGND: Ground pin.V1N: Voltage input pin.LBl, LB0: Low voltage input and output pins.PG: “Good” signal output pin.SW: Connect to the output inductor pin.