• Home
  • QUESTIONS & ANSWERS
  • Others
  • What are the principles for planning the IP address of an NE?

    * Question

    What are the principles for planning the IP address of an NE?


    *
    Answer

    Each network element must have a unique IP address.The network element can use standard IP addresses of categories A, B, and C.The IP address must be used with the subnet mask.A large PTN node on the core node and the backbone aggregation ring is configured as a gateway network element.The IP address of the non-gateway NE is recommended. Generally, no manual configuration is required.