* Question
What are the two types of drop-on-demand inkjet printing technology?
* Answer
Drop-on-demand (DOD) inkjet printing technology is classified into two main types based on the mechanism used to eject the ink droplets:
1. Thermal Inkjet (TIJ) Technology
Mechanism:
– Heating Element: Thermal inkjet printers use a tiny resistive heating element in each nozzle.
– Ink Ejection: When an electric current flows through the heating element, it rapidly heats up and vaporizes a small amount of ink, creating a bubble. The rapid expansion of this bubble forces a droplet of ink out of the nozzle and onto the printing substrate.
– Cooling and Refill: As the bubble collapses, it creates a vacuum that draws more ink into the nozzle from the reservoir, readying it for the next cycle.
Characteristics:
– Drop Formation: Produces precise and consistent droplets, typically in the range of 10 to 30 picoliters.
– Ink Types: Generally uses water-based inks, but can also handle other types like solvent-based inks.
– Resolution: Capable of high-resolution printing, suitable for text and images.
– Speed: Can achieve high print speeds due to the rapid heating and cooling cycles.
– Cost: Generally lower cost compared to piezoelectric printers, both in terms of initial purchase and consumables.
Applications:
– Widely used in consumer inkjet printers, office printers, and some industrial applications.
– Suitable for printing on paper, photo paper, and some types of specialty media.
2. Piezoelectric Inkjet (PIJ) Technology
Mechanism:
– Piezoelectric Crystal: Piezoelectric inkjet printers use a piezoelectric crystal located in each nozzle.
– Ink Ejection: When an electric voltage is applied to the crystal, it changes shape (deforms). This deformation creates a pressure pulse that forces a droplet of ink out of the nozzle.
– Versatility: The deformation is precisely controlled, allowing for the ejection of ink droplets of varying sizes.
Characteristics:
– Drop Formation: Can produce droplets of variable sizes, typically ranging from 1 to 50 picoliters or more.
– Ink Types: Compatible with a wider range of inks, including solvent-based, UV-curable, and pigment-based inks.
– Resolution: Capable of very high-resolution printing and precise control over ink deposition.
– Durability: Piezoelectric nozzles tend to have a longer lifespan since they do not undergo thermal stress.
– Cost: Higher initial cost and potentially higher cost of consumables compared to thermal inkjet technology.
Applications:
– Commonly used in industrial printing, commercial printing, and high-end desktop printers.
– Suitable for printing on a wide variety of substrates, including paper, plastics, textiles, ceramics, and metals.
– Thermal Inkjet (TIJ): Uses heat to create a bubble that ejects ink. It is cost-effective, suitable for high-resolution printing, and mainly used with water-based inks.
– Piezoelectric Inkjet (PIJ): Uses piezoelectric crystals to create pressure pulses that eject ink. It supports a broader range of inks and substrates, offers precise control, and is durable, but it is more expensive.
Both technologies have their unique advantages and are selected based on the specific requirements of the printing application.

COMMENTS