• Home
  • QUESTIONS & ANSWERS
  • Industrial Controls, Meters
  • What is an embedded controller?

    * Question

    What is an embedded controller?


    *
    Answer

    The embedded controller eliminates the need for an external PC, making the PXI chassis a complete system.Embedded controllers provide a wide range of standard and extended interfaces, such as serial, parallel, USB, mouse, keyboard, Ethernet, and GPIB interfaces.The embedded controller must be placed inside the system.The PXI embedded controller, as shown, has the advantage of being compact and easy to maintain.Most embedded controllers are 6U in size and some are 3U in size, occupying 1 to 4 slots.