* Question
| What is erasure? |
* Answer
| Erase refers to the operation of writing human data to the memory area in the chip.The memory of the chip is composed of E2PR()M, and the E2PROM has its own unique read/write mechanism, and erasing is the operation of writing 1.It should be specially pointed out that the erase operation is performed in a row, and an erase operation is performed on any one of the rows, and the result is that the entire row is erased. |

COMMENTS