• Home
  • QUESTIONS & ANSWERS
  • Others
  • What Is an Encapsulated VLAN ID?

    * Question

    What Is an Encapsulated VLAN ID?

    * Answer

    An encapsulated VLAN ID refers to the VLAN identifier that is inserted into a network frame as part of a VLAN tagging or encapsulation process. It is used to indicate which virtual LAN (VLAN) a specific data frame belongs to, enabling logical network segmentation over a shared physical infrastructure.

    1. Role of the VLAN ID

    The VLAN ID uniquely identifies a VLAN within a network.
    When traffic is transmitted across VLAN-aware devices such as switches or routers, the VLAN ID ensures that frames are forwarded only within the correct virtual network.

    2. VLAN ID Encapsulation in Ethernet Frames

    In most Ethernet-based networks, VLAN encapsulation follows the IEEE 802.1Q standard.
    A VLAN tag is inserted into the Ethernet frame header, and this tag contains the VLAN ID field. The encapsulated VLAN ID is carried inside this tag along with priority and control information.

    3. Purpose of Encapsulation

    Encapsulating the VLAN ID allows:

    • Multiple VLANs to share the same physical network links
    • VLAN information to be preserved across trunk links
    • Network devices to apply VLAN-based forwarding and security policies

    Without encapsulation, VLAN information would be lost during frame transmission.

    4. Scope and Value Range

    The VLAN ID field typically supports values from 1 to 4094.
    Certain values are reserved for system use, while others are assigned to user-defined VLANs based on network design requirements.

    5. Application Scenarios

    Encapsulated VLAN IDs are commonly used in:

    • Ethernet trunk links between switches
    • Industrial Ethernet and automation networks
    • Data center and enterprise network segmentation

    Summary

    An encapsulated VLAN ID is the VLAN identifier embedded within a tagged Ethernet frame to indicate its VLAN membership. By encapsulating the VLAN ID, networks can support logical segmentation, improved traffic management, and scalable multi-VLAN communication over shared physical links.

    COMMENTS

    WORDPRESS: 0
    DISQUS: 0