• Home
  • QUESTIONS & ANSWERS
  • Resistors
  • What is the precision chip Resistors?

    * Question

    What is the precision chip Resistors?


    *
    Answer

    Care should be taken to prevent thermistor from heating up due to heating.Thermal time constant: τ [sec.] The thermistor changes the temperature of the thermistor itself due to the step effect under the zero energy condition. The time required for the temperature to change 63.2% between the initial value and the final value isThermal time coefficient τ.Care should be taken to prevent thermistor from heating up due to heating.

    Thermal time constant: τ [sec.] The thermistor changes the temperature of the thermistor itself due to the step effect under the zero energy condition. The time required for the temperature to change 63.2% between the initial value and the final value isThermal time coefficient τ.Domestic customers: Taiwan Proview Technology, Anke, Shunda Computer, Xu Li, Dongguan Phillips, Nantai, Flextronics, Tamura, etc.