* Question
What is the working principle of the contact logic encryption card?
* Answer
The working principle of a contact logic encryption card involves using a secure, embedded
microcontroller or chip that interacts with an external reader through physical contact. This card
is often used for secure authentication, encryption, and data storage, commonly found in
applications such as banking cards, identification, and access control systems.
Here’s an overview of its working principle:
1. Physical Contact Interface
– The card contains a set of contact pads (gold-plated terminals) that establish a physical
connection with the card reader when inserted into a reader device.
– Once contact is made, the reader powers the card and establishes communication using a
defined protocol (e.g., ISO/IEC 7816 standard for smart cards).
2. Microcontroller and Secure Chip
– Inside the card, a microcontroller or secure chip manages all operations, including data
processing, encryption, and storage.
– The card contains logic circuitry that controls how data is accessed, ensuring that only
authorized requests are processed, protecting sensitive information.
3. Authentication Process
– When a user inserts the card into a reader, the card and the reader undergo a mutual
authentication process. The reader sends a challenge to the card, and the card responds with
encrypted data or a digital signature using its internal cryptographic algorithms (such as RSA, DES,
AES).
– The card typically stores encryption keys or digital certificates that are securely generated and
stored during manufacturing. The challenge-response mechanism ensures that both the card and
reader authenticate each other.
4. Encryption and Data Exchange
– The card securely encrypts or decrypts information using its embedded cryptographic
algorithms. All data exchanged between the card and the reader is protected through encryption
to prevent interception or tampering.
– Depending on the application, the card may handle different types of encryption functions,
such as symmetric (e.g., AES) or asymmetric (e.g., RSA) encryption for secure communication.
5. Access Control and Logic Functions
– The logic encryption card has built-in access control mechanisms that restrict unauthorized
access to its data. It uses logic circuits to decide how to handle different requests, such as
granting access to certain data or triggering additional security checks.
– The logic in the card can verify the identity of the cardholder through PIN codes, biometrics, or
digital certificates before allowing any sensitive data transactions.
6. Data Storage and Security
– The card stores sensitive data (such as user credentials, account information, or cryptographic
keys) in secure, non-volatile memory. This data is usually protected against tampering,
unauthorized access, and cloning through multiple layers of security mechanisms.
– Secure elements inside the card ensure that data is erased or rendered useless if tampering is
detected.
7. Execution of Secure Operations
– After authentication, the card can perform a variety of secure operations, such as generating
digital signatures, encrypting data, or facilitating transactions. These operations are securely
processed within the card, ensuring data confidentiality and integrity.
– For example, in a banking card application, the card might generate a dynamic code for
transaction verification, ensuring the security of each transaction.
8. Power Supply
– The card receives power from the contact with the reader. Once inserted, the reader provides
the necessary power to activate the internal circuitry of the card.
9. End-to-End Security
– Throughout the process, encryption cards use secure cryptographic algorithms and hardware
security measures to ensure end-to-end security. The card’s logic ensures that all communication
between the card and the reader remains protected, mitigating risks like data interception,
cloning, or fraud.
In summary, the contact logic encryption card operates by establishing a physical connection with
a reader, processing data securely using cryptographic algorithms, and controlling access through
logic circuits. It ensures authentication, encryption, and secure data exchange, making it highly
secure for applications like banking and identity verification.

COMMENTS