Schottky Diode: How It Works, Where It’s Used, and How to Pick One

  • Home
  • SUPPLY CHAIN INSIGHTS
  • Schottky Diode: How It Works, Where It’s Used, and How to Pick One

    The Schottky diode has been a staple of power electronics for decades, and for good reason. Its metal-semiconductor junction gives it two properties that standard PN diodes simply cannot match at the same time: a very low forward voltage drop and an extremely fast switching response. Those two characteristics, taken together, explain why you will find Schottky diodes in switching power supplies, RF circuits, solar panel bypass strings, and automotive battery management systems alike.

    This article covers what a Schottky diode actually is and how its junction works, how it compares to a conventional diode, the electrical specifications that matter most when reading a datasheet, the applications where it performs best, and a practical framework for picking the right device for a given design. Silicon carbide (SiC) variants are also covered, as they have become increasingly relevant in high-power and high-efficiency applications over the past several years.

    Electronics Deep Dive
    Schottky Diode

    How It Works, Where It’s Used & How to Pick One — the essential visual reference for engineers and procurement teams.

    ★ 5 Key Takeaways
    1

    Metal-semiconductor junction eliminates minority carrier storage for near-zero reverse recovery.

    2

    Forward voltage of 0.15–0.45 V vs. 0.6–0.7 V for silicon PN diodes — cuts conduction losses significantly.

    3

    Sub-10 ns switching speed makes Schottkys ideal for SMPS, RF, and high-frequency designs.

    4

    Si Schottkys top out near 200 V; SiC variants push to 600–1700 V with the same majority-carrier advantage.

    5

    Selection rule of thumb: VRRM ≥ 1.3× peak reverse voltage; IF(AV) at ≤60% of rating.

    Schottky vs. Standard PN Diode
    Parameter Schottky PN Diode
    Forward Voltage (VF) 0.15–0.45 V ✓ 0.6–0.7 V
    Switching Speed <10 ns ✓ 100–1000 ns
    Reverse Recovery (Qrr) ~Zero ✓ Significant
    Max Reverse Voltage (Si) <200 V High ✓
    Reverse Leakage (IR) Higher (temp-sensitive) Lower ✓

    Forward Voltage Drop Comparison
    Si Schottky (low)
    0.15 V
    Si Schottky (high)
    0.45 V
    Si PN Diode
    0.6–⁠0.7 V
    Fast-⁠Recovery PN
    ≥1.0 V

    Lower VF = lower conduction losses = better efficiency, especially in low-voltage rails (3.3 V / 5 V).

    How the Junction Works
    1
    Metal–Semiconductor Contact

    Metal (Mo, Al, Pt, or W) contacts lightly doped N-type silicon. Electrons redistribute to equalize Fermi levels, forming the Schottky barrier and a depletion region.

    2
    Forward Bias: Hot Carriers

    Forward bias narrows the barrier. Majority-carrier electrons — called “hot carriers” — cross directly into the metal. No minority carriers are injected, so no reverse recovery charge is stored.

    3
    Reverse Bias: Fast Block

    Reverse bias widens the barrier. Switching off is limited only by junction capacitance discharge — measured in nanoseconds or hundreds of picoseconds in small-signal types.

    Where Schottky Diodes Are Used
    ⚡
    Switching Power Supplies

    Output rectifiers & freewheeling diodes in buck/boost converters at 100 kHz–MHz

    ☀️
    Solar PV Systems

    Bypass & blocking diodes on cell strings; low VF minimizes generation losses

    RF & Microwave

    Mixers, detectors, clamps in radar, cellular, Wi-Fi & Bluetooth front ends

    Automotive

    Battery isolation, reverse polarity & load dump protection; EV/HEV traction stages (SiC)

    Digital & Mixed-Signal

    Transistor saturation clamping, I/O voltage limiting, power OR-ing with redundant supplies

    6 Specs to Check on the Datasheet
    VRRM
    Peak Reverse Voltage

    Select ≥1.3× worst-case reverse voltage including inductive spikes. Higher ratings raise VF, so balance matters.

    IF(AV)
    Avg Forward Current

    Operate at ≤60% of rated IF(AV). Also verify surge current (IFSM) covers start-up or fault inrush.

    VF
    Forward Voltage Drop

    Evaluate from the VF vs. IF curve at your actual operating current — not just the datasheet headline figure.

    IR
    Reverse Leakage

    Rises exponentially with temperature. Check the hot-condition IR curve — high leakage at temp can trigger thermal runaway.

    Tj(max)
    Max Junction Temp

    Combined with RθJA/RθJC thermal resistance, sets the maximum dissipation limit in a given PCB/heatsink configuration.

    Cj
    Junction Capacitance

    Low-pF range in Schottky devices; critical for RF mixers, detectors, and high-frequency switching circuits.

    SiC Schottky Diodes: Pushing the Voltage Ceiling

    Silicon Carbide — a wide-bandgap material with ~10× the critical field of silicon — extends Schottky majority-carrier advantages into kilovolt-class power electronics.

    600–
    1700 V
    Commercial SiC SBD breakdown voltage range
    ~Zero
    Qrr retained even at kilovolt ratings — silicon PIN diodes cannot match this
    PFC / EV
    Key SiC use cases: PFC boost stages, 3-phase inverters, EV on-board chargers & traction drives

    Key SiC families: Infineon thinQ! · STMicroelectronics STPSC · ON Semiconductor FFSP (600 V–1200 V range)

    Selection Checklist: 4-Step Framework
    1
    Set Reverse Voltage Margin

    Find worst-case reverse voltage (including spikes) → choose VRRM ≥ 1.3× that value. Example: 70 V spikes on a 48 V bus → select 100 V rated device.

    2
    Derate the Current Rating

    Operate at ≤60% of IF(AV). Confirm IFSM surge rating covers inrush. Account for actual PCB thermal environment, not datasheet test conditions.

    3
    Evaluate VF at Real Operating Point

    Read the VF vs. IF curve at your actual current and temperature — the datasheet headline figure is typically at rated max current.

    4
    Check IR at Elevated Temperature

    If Tj >50–60°C, review the hot-condition leakage curve. Consider trench-structure Schottky types for thermally demanding designs to avoid runaway.

    Common Packages & Reference Parts
    By Power Level
    Small-signal / Low-ISOD-123, SOD-323, SOT-23
    Medium-power SMTSMA, SMB, SMC
    High-power SMPSTO-220, D2PAK, TO-247
    Reference Part Families
    1N5817/18/1920–40 V, 1 A, DO-41 (TH)
    SS14 / SS34 / SS541–5 A, 40 V, SMA
    BAT54Small-signal single & dual, SOT-23
    MBR340 / MBR3603 A, 40–60 V, TO-220

    Need Schottky Diodes or Discrete Semiconductors?

    WIN SOURCE is a global independent distributor of electronic components, supporting component supply, shortage sourcing, lifecycle management and alternative solutions.

    Submit RFQ / BOM →
    AS9120 CertifiedISO 9001ERAI Member#15 Global — Supply Chain Connect 2026win-source.net

    What Is a Schottky Diode?

    A Schottky diode, formally called a Schottky Barrier Diode (SBD), is a semiconductor diode built around a metal-to-semiconductor junction rather than the P-N junction used in conventional diodes. The junction is formed by placing a metal — typically molybdenum, aluminum, platinum, or tungsten — in contact with a lightly doped N-type semiconductor substrate. This contact creates a potential energy barrier at the interface, known as the Schottky barrier, which governs how the device conducts and blocks current. Because the metal forms the anode and the N-type semiconductor forms the cathode, the structure is fundamentally different from anything built by joining two semiconductor regions together.

    The device is named after German physicist Walter H. Schottky, whose theoretical work on metal-semiconductor interfaces laid the groundwork for practical barrier diodes. It is also known informally as a hot-carrier diode or surface barrier diode, names that reflect the high-energy electrons involved in its conduction mechanism. Today, SBDs are manufactured by virtually every major discrete semiconductor supplier and are available in current ratings from milliamps to tens of amps, covering a wide range of package styles and voltage classes.

    How It Works: The Metal-Semiconductor Junction

    When the metal and N-type semiconductor are brought into contact, electrons near the interface redistribute themselves to equalize the Fermi levels of the two materials. This redistribution creates a depletion region in the semiconductor just beneath the metal surface, and the resulting built-in electric field forms the Schottky barrier. Because the barrier height in a metal-semiconductor junction is lower than the built-in potential of a comparable PN junction, less forward voltage is required to push electrons across it — which is the root cause of the diode’s characteristically low forward voltage drop.

    When forward bias is applied (anode positive with respect to cathode), the barrier narrows and majority-carrier electrons in the semiconductor gain enough energy to cross into the metal, producing forward current. These electrons are called “hot carriers” because they carry more kinetic energy than thermally equilibrated electrons in a standard PN junction. This is why the device conducts at a forward voltage typically between 0.15 V and 0.45 V, compared to approximately 0.6 V to 0.7 V for a silicon PN junction diode. When reverse bias is applied, the barrier widens, internal resistance increases sharply, and current ideally ceases to flow — though in practice a small reverse leakage current is always present.

    A critical consequence of this majority-carrier mechanism is that there are no minority carriers stored near the junction during forward conduction. In a PN diode, minority carriers injected across the junction must be swept out or recombine before the diode can block reverse current — a process that takes time and produces the reverse recovery charge (Qrr). Because the Schottky diode uses only majority carriers, this charge storage problem is essentially eliminated. The switching transition from forward-conducting to reverse-blocking is governed instead by the discharge of the junction’s own capacitance, which occurs in nanoseconds or even hundreds of picoseconds in small-signal devices.

    Schottky Diode vs. PN Junction Diode

    The differences between a Schottky diode and a standard PN junction diode flow directly from their structural differences. The most significant practical advantage is the forward voltage drop: a silicon Schottky diode typically turns on at around 0.2 V to 0.45 V, whereas a silicon PN diode requires roughly 0.6 V to 0.7 V, and fast-recovery rectifiers can reach 1.0 V or more at high current densities. In a low-voltage supply — say, a 3.3 V or 5 V rail — even a 0.3 V reduction in rectifier drop translates directly into measurable efficiency improvement and less heat to manage.

    The switching speed difference is equally significant. Reverse recovery time in standard PN rectifiers is measured in hundreds of nanoseconds; fast-recovery diodes bring that down to under 100 ns; Schottky diodes can switch in under 10 ns, and small-signal types achieve sub-nanosecond transitions. This matters in any circuit where the diode switches at high frequency — the switching losses in a PN diode operating at several hundred kilohertz can represent a meaningful fraction of total power loss, while those losses are negligible in a Schottky device.

    The trade-offs run in the opposite direction when it comes to reverse voltage and leakage. Standard silicon Schottky diodes are generally limited to reverse blocking voltages below 200 V, with most general-purpose types rated between 20 V and 100 V. Reverse leakage current is also higher than in a PN diode, and it increases strongly with junction temperature — making thermal management more important and raising the risk of thermal runaway if the operating environment is not well characterized. These limitations define where Schottky diodes are suitable and where conventional or fast-recovery PN diodes remain the better choice.

    Key Electrical Specifications

    Reading a Schottky diode datasheet efficiently requires understanding what each parameter actually controls in a real circuit. The following are the specifications that most directly determine whether a device will work correctly and reliably in a given application.

    • VRRM — Peak Repetitive Reverse Voltage: The maximum reverse voltage the diode can sustain repeatedly without breakdown. Inductive switching circuits generate voltage spikes that can significantly exceed the nominal rail voltage, so selecting VRRM with a safety margin of at least 30% above the worst-case reverse voltage is a common design rule. Selecting an excessively high rating, however, increases both forward voltage and cost, so balance matters.
    • IF(AV) — Average Forward Current: The maximum continuous forward current at rated temperature. The actual operating current should generally be kept to no more than 60% of the rated value to ensure thermal stability and adequate derating margin.
    • VF — Forward Voltage Drop: Always evaluate this at the actual operating current, not just the datasheet headline figure. VF is specified at a particular current, and the real drop at lighter loads will be lower; at heavy loads or high temperatures it can rise. This directly affects conduction loss and thermal load.
    • IR — Reverse Leakage Current: Specified at a given reverse voltage and junction temperature. Because leakage increases exponentially with temperature, always check the hot-condition figure if the device will see elevated temperatures in service. High leakage in standby mode can be a significant issue in battery-powered or energy-sensitive applications.
    • Tj(max) — Maximum Junction Temperature: Sets the absolute thermal ceiling for the device. Combined with the thermal resistance from junction to case or ambient (RθJA, RθJC), this determines how much power the device can dissipate in a given PCB or heatsink configuration before it exceeds its safe operating limit.
    • Cj — Junction Capacitance: Relevant in RF and high-frequency switching applications. Schottky junctions are typically small, keeping capacitance in the low picofarad range, which contributes to their fast switching and suitability for signal detection and mixing circuits.

    Datasheets from manufacturers like Infineon, STMicroelectronics, ON Semiconductor, and Vishay present these parameters in standardized tables and characteristic curves. When in doubt about any parameter, the application curves — particularly VF vs. IF and IR vs. temperature — are more informative than the single-point header values.

    Where Schottky Diodes Are Used

    The combination of low forward voltage and fast switching has made Schottky diodes nearly universal in low-voltage power conversion. In switching power supplies (SMPS), they serve as output rectifiers and freewheeling diodes in buck and boost converter topologies, where the ability to switch cleanly at frequencies from 100 kHz to several megahertz is essential. A conventional PN diode’s reverse recovery charge would generate excessive switching losses and EMI at those frequencies; a Schottky’s near-zero Qrr sidesteps the problem entirely. The same principle applies in synchronous rectifier bypass diodes, where the Schottky provides a low-loss current path during dead time.

    In solar photovoltaic systems, Schottky diodes are used as bypass diodes across individual cell strings and as blocking diodes between the panel and the battery or inverter. The blocking diode function is straightforward: during periods of low light or at night, the panel’s voltage falls below the battery voltage, and a diode in series prevents the battery from discharging back through the panel. The Schottky’s low forward drop minimizes the power lost through the blocking diode during normal operation, which matters across thousands of hours of annual generation.

    RF and microwave applications represent a distinct but equally important use category. Schottky diodes are used in frequency mixers, signal detectors, and clamp circuits in radio receivers, radar front ends, microwave ovens, and wireless communication modules including those handling cellular, Wi-Fi, and Bluetooth signals. Their small junction capacitance and fast carrier response allow them to follow signal transitions at gigahertz frequencies where any minority carrier storage would be completely prohibitive. Specialized GaAs-based Schottky diodes extend this performance into millimeter-wave frequencies.

    In digital and mixed-signal circuits, Schottky diodes are used to clamp transistor saturation, limit voltage spikes on I/O lines, and implement OR-gate power steering (commonly called power OR-ing) in systems with redundant supplies. In automotive electronics, they appear in battery isolation circuits, reverse polarity protection, and load dump protection, where the combination of low drop, fast response, and mechanical robustness in compact packages is valued. Electric vehicles and hybrid powertrains have added demand at higher current levels, which has driven adoption of SiC variants in those traction power stages.

    SiC Schottky Diodes: Pushing the Voltage Ceiling

    One of the most significant limitations of standard silicon Schottky diodes is the reverse voltage ceiling. Because the thin Schottky barrier breaks down relatively easily under high reverse fields, practical silicon SBDs are generally limited to breakdown voltages below 200 V, with most commodity types rated at 100 V or less. This restriction has historically excluded Schottky diodes from high-voltage power conversion stages in motor drives, inverters, and grid-tied power electronics, where PN junction diodes or IGBTs were the only viable options despite their slower switching and higher losses.

    Silicon carbide (SiC) changes that picture. SiC is a wide-bandgap semiconductor with a critical electric field strength roughly ten times that of silicon, which means a SiC Schottky diode can sustain much higher reverse voltages within a much thinner drift region. SiC SBDs with breakdown voltages in the 600 V to 1700 V range are now commercially available from multiple suppliers, and devices rated at 3300 V are also in production for the most demanding industrial applications. Crucially, these high-voltage SiC devices retain the majority-carrier conduction mechanism, so they maintain near-zero reverse recovery charge even at kilovolt ratings — a capability that silicon PIN diodes at comparable voltages simply cannot match.

    The practical impact is substantial. SiC Schottky diodes are now widely used as boost diodes in power factor correction (PFC) stages, in the freewheeling position of three-phase inverter bridges, and in EV on-board chargers and traction inverters. Their low switching losses allow converter operating frequencies to increase without proportional increases in switching loss, enabling smaller magnetics and passive components throughout the system. The trade-off remains the cost premium relative to silicon devices, though that gap has been narrowing steadily as SiC wafer production has matured.

    How to Select a Schottky Diode

    Selecting a Schottky diode for a specific application is a straightforward process once you have a clear picture of the electrical environment the device will operate in. The goal is to match the device’s ratings to the circuit’s demands with appropriate margins, without over-specifying in ways that introduce unnecessary cost or increased forward drop.

    Start with the reverse voltage. Determine the maximum reverse voltage the diode will see in normal operation, including any inductive transients or switching spikes, then choose a device whose VRRM exceeds that value by at least 30%. In a 48 V bus converter with transient spikes reaching 70 V, for instance, a 100 V rated device provides adequate headroom. Avoid going much higher than necessary, since forward voltage tends to increase with higher voltage ratings, and that costs efficiency.

    Next, establish the current requirement. Identify the average forward current IF(AV) and the peak or surge current the device must handle during start-up or fault conditions. Rate the device so the nominal operating current is no more than 60% of its rated IF(AV), accounting for the actual PCB thermal environment rather than the datasheet’s idealized test conditions. Check the surge current rating (IFSM) against the application’s worst-case inrush.

    Then evaluate VF at the actual operating current and temperature. The forward voltage figure listed at the top of a datasheet is usually measured at a specific current — often the rated maximum — and the shape of the VF vs. IF curve at your operating point may look quite different. This is particularly important in low-voltage rails where even 50 mV of extra drop represents a non-trivial efficiency cost.

    Finally, check reverse leakage at elevated temperature. If the device will operate above 50°C or 60°C, look at the IR vs. temperature curve rather than just the room-temperature figure. High leakage at temperature can cause self-heating, which increases leakage further — a feedback loop that, in extreme cases, leads to thermal runaway. Trench-structure Schottky diodes are specifically designed to reduce leakage while maintaining low forward drop, and they are worth considering in thermally challenging environments.

    Common Packages and Part Families

    Schottky diodes are available in a wide range of packages suited to different power levels and PCB mounting requirements. Small-signal and low-current devices typically come in SOD-123, SOD-323, SOT-23, and similar surface-mount packages, with dual-diode configurations (common cathode or common anode) also standard in SOT-23 and SOT-363 outlines. Medium-power rectifier types are commonly found in SMA (DO-214AC), SMB (DO-214AA), and SMC (DO-214AB) packages. Higher-power devices for SMPS output stages use TO-220, TO-263 (D2PAK), and TO-247 packages, the latter often in dual common-cathode configurations that allow a single package to rectify a full push-pull secondary.

    Some widely referenced part families worth knowing include the 1N5817/1N5818/1N5819 series (20 V / 30 V / 40 V, 1 A, through-hole DO-41) as classic general-purpose types. The SS14, SS34, and SS54 families offer 1 A, 3 A, and 5 A current ratings at 40 V in SMA packages and are common in modern SMT designs. The BAT54 family provides small-signal single and dual diodes in SOT-23 for clamping and logic steering. At higher currents, the MBR340 (3 A, 40 V) and MBR360 (3 A, 60 V) are long-established benchmark types in TO-220 and surface-mount versions. For SiC applications, families from Infineon (thinQ! series), STMicroelectronics (STPSC series), and ON Semiconductor (FFSP series) cover the 600 V to 1200 V range.

    When sourcing any of these devices, it is worth verifying that package dimensions, pad layouts, and lead finish specifications match the original design intent, particularly when moving between manufacturers. Minor variations in thermal resistance, forward voltage tolerance, or leakage specification between approved manufacturers can affect system-level performance more than the datasheet header values suggest. Where a cross-reference produces a candidate from a different manufacturer, final approval belongs to the customer’s engineering team — a parametric match on the header values is necessary but not sufficient.

    Final Thoughts

    The Schottky diode is one of those components whose value becomes immediately clear once you understand the physics behind it. The metal-semiconductor junction eliminates minority carrier storage, cuts the forward voltage drop roughly in half compared to a silicon PN diode, and pushes switching speed into the nanosecond range. Those three properties together explain its presence in nearly every modern switching power supply, RF front end, and solar energy system in production today. SiC variants have extended the same majority-carrier advantages into kilovolt-class power electronics, opening up applications that silicon Schottky technology was never able to address.

    Selecting the right device comes down to matching VRRM, IF(AV), VF, and IR to the actual circuit conditions with appropriate derating margins, and understanding how temperature affects each of those parameters. A little time spent on the characteristic curves in the datasheet usually pays off more than any rule of thumb.

    Sourcing these devices is a question that runs the length of a product’s life — prototype builds, volume production, and the years after a part family is withdrawn while a fielded design still has to be supported. WIN SOURCE is a global independent distributor of electronic components, supporting component supply, shortage sourcing, lifecycle management and alternative solutions, with inventory across standard, hard-to-find and end-of-life discrete semiconductors from manufacturers including Infineon, STMicroelectronics, ON Semiconductor and Vishay.

    Frequently Asked Questions

    What is the main advantage of a Schottky diode over a standard diode?

    Two things at once: a forward voltage drop of roughly 0.15–0.45 V against 0.6–0.7 V for a silicon PN diode, and effectively zero reverse recovery charge. The lower drop cuts conduction loss, which matters most on low-voltage rails, and the absence of stored minority carriers means the device switches off in nanoseconds rather than hundreds of nanoseconds. That combination is why Schottky diodes dominate low-voltage switching power supplies.

    What is the typical forward voltage drop of a Schottky diode?

    Silicon Schottky diodes generally turn on between about 0.15 V and 0.45 V, depending on the device and the current at which it is measured. Always read the figure off the VF vs. IF curve at your actual operating current and temperature rather than taking the datasheet headline number, which is usually quoted at the rated maximum current.

    Why are silicon Schottky diodes limited to low reverse voltages?

    The thin Schottky barrier breaks down relatively easily under a high reverse field, so practical silicon devices are generally limited to breakdown voltages below 200 V, and most commodity parts are rated at 100 V or less. Silicon carbide changes this: its critical field strength is roughly ten times that of silicon, so SiC Schottky diodes reach the 600 V to 1700 V range while keeping the same near-zero reverse recovery.

    When should I use a PN diode instead of a Schottky?

    When you need high reverse blocking voltage, low reverse leakage, or operation at elevated temperature where leakage would otherwise run away. Schottky leakage rises exponentially with junction temperature, and a standard silicon PN or fast-recovery diode is the better choice above the Schottky voltage ceiling or in thermally demanding, low-duty-cycle positions where switching speed does not matter.

    What should I check before substituting one Schottky diode for another?

    Compare VRRM, IF(AV), IFSM, the VF curve at your operating point, the IR curve at temperature, and the thermal resistance of the package, then confirm the package outline, pad layout and lead finish match the board. A parametric match on the header values is not enough, and final approval of any substitution belongs to your engineering team.

    Part discontinued, obsolete or hard to find?

    WIN SOURCE is a global independent distributor of electronic components, supporting component supply, shortage sourcing, lifecycle management and alternative solutions. Visual inspection, non-destructive testing and electrical testing are applied according to material risk, customer requirements and the applicable quality process, and orders are covered by the published return policy and a 3-year warranty on eligible components.

    Stock and pricing are updated daily — search a part number or contact us for current availability, lead time and a quote.

    Search a Part Number  Upload a BOM / RFQ

    © 2026 Win Source Electronics. All rights reserved. This content is protected by copyright and may not be reproduced, distributed, transmitted, cached, or otherwise used without the prior written permission of Win Source Electronics.