What is the purpose of active PFC technology? The purpose of active PFC technology is to improve the input power…

What constitutes an airbag protection system? It is generally composed of a sensor, a controller (ECU), a gas generator, an…

What is a mutual sensor? A sensor that converts the measured non-electricity change into a change in the mutual inductance…

What are the commonly used bulk data load/store instructions? LDM—Bulk Data Load Instructions and STM—Batch Data Store Instructions. What is…

What are the steps for CAN to handle errors when an error occurs? Detect whether it is a local (Local)…

Which modules are the multi-function password locks divided into? The multi-function password lock is divided into three modules: a frequency…

The difference between inductance and resistance: The inductor belongs to the passive component and only works when the current passes.Its…

When did you enter the exception mode? After entering the management mode after the processor reset, the operating system kernel…

What are the characteristics of the I2C interface? Standard I2C bus interface; configurable as master, slave, or master/slave; programmable clock…