What is the HART standard? The HART standard (WWW.hartcomm.org) was formulated in the late 1980s.In its initial version, the HART…

What constitutes a remote frame? A long-range frame is composed of 6 different bit fields: frame start, arbitration field, control…

What are the advantages of KMV power control? Reduce costs. Improve business continuity. Not limited to hardware platform and operating…

What is SJAl000? SJAl000 is a stand-alone CAN controller with advanced features for automotive and general industrial applications.It is an…

What are the main technical features of the MAX7316? 400kbit/s, 2-wire serial interface, 5.5V voltage tolerance; Working voltage is 2~3.6V;…

What is real-time 3D visualization? Through real-time 3D visualization, the water environment information can be effectively and intuitively presented to…

Briefly describe the bit arbitration technology of CAN? CAN’s non-destructive bit arbitration technology is different from general arbitration technology.In general…

What are the management functions provided by the Central Coordination Station (CCo)? The new site joins AV1. Coordination of N;…