• Home
  • Tutorials
  • Ten Daily Electronic Common Sense-Section 7

    What are the architectures of embedded systems?

    The architecture of embedded systems is from the bottom up, generally divided into: hardware, drivers, operating systems, API interfaces, applications

    What are the applications of the counter?

    The counter is the most widely used sequential logic circuit, and is often used for timing, timing, delay, frequency division of digital systems and the formation of sequential pulse generators.

    How to classify the OTG link core register (base address 7C000000h)?

    Core global register; host mode register; device mode register

    What parts of the initialization of MSCAN include?

    1. Select the microcontroller in the CONFIG2 as the AZ series and allow the MSCAN to work.
    2. Set the basic working mode of MSCAN in CMCR0 and CMCR1.
    3. Select the method of MSCAN filtering identifiers in CIDAC, and set the acceptance code and mask bit in CIDAR0~CIDAR3 and CIDMR0~CIDMR3 respectively.
    4. Set the bit timing logic of MSCAN in CBTR0 and CBTR1 to determine the communication bit rate.
    5. In CRIER and CTCR, the relevant interrupts are set to be allowed to occur.
    6. Start the MSCAN module.

    What are the procedural assignments in Verilog HDL?

    In Verilog HDL, there are two procedural assignments, blocking and nonblocking.

    What are the advantages of a conversion element made using the eddy current effect?

    The advantages of the conversion element made by the eddy current effect are: high sensitivity, simple structure, strong anti-interference ability, no influence of oil and other medium, and non-contact measurement.

    What are the main characteristics of photocells?

    The basic characteristics of photocells are: volt-ampere characteristics, photoelectric properties and spectral properties.

    What are the new semiconductor devices that Zetex focuses on?

    Zetex focuses on adapting to these unique new semiconductor devices, including bipolar transistors, MOSFETs, Schottky diodes, current monitoring devices, and low-power current regulators.

    What is the piezoresistive effect?

    After the single crystal silicon material is subjected to stress, its resistivity changes significantly. This phenomenon is called piezoresistive effect.

    Briefly describe the logic function of the CMOL circuit?

    The logic function of the CMOL circuit mainly depends on the underlying CMOS circuit unit, which consists of an inverter and two pass transistors, where the pass transistors are used for the input and output of the CMOS unit circuit.
    Two-pass transistors are connected to the output nanowire and the input nanowire, respectively, and are used as pull-up or pull-down resistors.
    The “OR” logic is realized between the upper two layers of nanowires through molecular devices, and the bottom CMOS single-channel unit realizes “NO” logic, so the CMOL circuit only realizes a single NOR logic function.
    In the CMOL circuit, through the two-layer nanowire array and the underlying CMOS inverter circuit, the realization of the circuit logic function is very simple.
    As long as the molecular device between the output nanowire of the output unit participating in the NOR logic operation and the corresponding input nanowire is in the “ON” state, the NOR logic between the corresponding CMOS units can be realized.