* Question
| What is the purpose of the capacitor? |
* Answer
| There are many uses for capacitors, mainly as follows:
1.DC blocking: The role is to prevent DC from passing and let the AC pass. 2.Bypass (decoupling): Provides a low impedance path for some of the parallel components in the AC circuit..Temperature compensation: compensates for the influence of other components on the temperature, and compensates to improve the stability of the circuit. 6.Timing: Capacitors are used in conjunction with Resistorss to determine the time constant of the circuit. 7.Tuning: System tuning of frequency-dependent circuits such as cell phones, radios, and televisions. |

COMMENTS