Ten Daily Electronic Common Sense-Section 148
What is the main reason for the mechanical lag?
After the strain gauge is subjected to mechanical strain, there will be residual deformation i [...]

Ten Daily Electronic Common Sense-Section 147
What is on the fixed length and the slider winding?
There are three sets of planar windings of thick, medium and thin on the fixed-length and [...]

Ten Daily Electronic Common Sense-Section 146
What are the common VHDL statements?
VHDL commonly used statements are divided into two types: parallel (Concurrent) statements and sequential [...]

Ten Daily Electronic Common Sense-Section 145
What are the main functions of the network layer?
It manages and assigns network addresses, automatically formulates and maintains network rou [...]

Ten Daily Electronic Common Sense-Section 144
What is the temperature difference potential?
The electric field hinders the further diffusion of electrons. When dynamic equilibrium is reach [...]

Ten Daily Electronic Common Sense-Section 143
What are the challenges of implementing embedded processor peripheral design based on SOPC Builder?
Embedded processor interfaceSystem process [...]

Ten Daily Electronic Common Sense-Section 142
What are the ways in which message mailboxes work?
One-to-one working method: This working method means that one task sends a message to the m [...]

Ten Daily Electronic Common Sense-Section 141
What is the HART standard?
The HART standard (WWW.hartcomm.org) was formulated in the late 1980s.In its initial version, the HART field commun [...]

Ten Daily Electronic Common Sense-Section 140
What constitutes a remote frame?
A long-range frame is composed of 6 different bit fields: frame start, arbitration field, control field, CRC [...]

Ten Daily Electronic Common Sense-Section 139
What are the advantages of KMV power control?
Reduce costs.Improve business continuity.Not limited to hardware platform and operating system.
[...]