Ten Daily Electronic Common Sense-Section 138
What is SJAl000?
SJAl000 is a stand-alone CAN controller with advanced features for automotive and general industrial applications.It is an al [...]

Ten Daily Electronic Common Sense-Section 137
What are the main technical features of the MAX7316?
400kbit/s, 2-wire serial interface, 5.5V voltage tolerance;Working voltage is 2~3.6V;8-bi [...]

Ten Daily Electronics Common Sense-Section 136
What is real-time 3D visualization?
Through real-time 3D visualization, the water environment information can be effectively and intuitively p [...]

Ten Daily Electronic Common Sense-Section 135
What is the way to detect roads?
Turn on the ignition switch, do not start the engine, and use a multimeter to check whether there is voltage [...]

Ten Daily Electronic Common Sense-Section 134
Briefly describe the bit arbitration technology of CAN?
CAN's non-destructive bit arbitration technology is different from general arbitration [...]

Ten Daily Electronic Common Sense-Section 133
What are the management functions provided by the Central Coordination Station (CCo)?
The new site joins AV1. Coordination of N;New sites join [...]

Ten Daily Electronic Common Sense-Section 132
What are the commonly used random access memories?
Static RAM (SRAM): The characteristic of static RAM is that it can reliably maintain the st [...]

Ten Daily Electronic Common Sense-Section 131
What is the control of high resolution enhanced pulse width modulation?
Controlled by three 8-bit high-resolution registers.These high-resolut [...]

Ten Daily Electronic Common Sense-Section 130
What is included in the signal channel section?
The input of the measured signal channel 1 and the measured signal channel 2 are used to acces [...]

Ten Daily Electronic Common Sense-Section 129
What is the detection method of the photoelectric crank position sensor?
Unplug the sensor plug, turn on the ignition switch, and check that t [...]