Ten Daily Electronic Common Sense-Section 8
What are the registers in the ARM state?
In the ARM state, the 16 general-purpose registers RO and Rl5 and one or two status registers (CPSR a [...]

Ten Daily Electronic Common Sense-Section 7
What are the architectures of embedded systems?
The architecture of embedded systems is from the bottom up, generally divided into: hardware, [...]

Ten Daily Electronic Common Sense-Section 6
What are the two basic forms of reset operation?
Power-on reset and power-on or switch reset.The power-on reset requires a reset operation aft [...]

Ten Daily Electronic Common Sense-Section 5
How to configure and modify the network of TQ2440 development board?
Modify the network configuration file /etc/net.Conf, which contains infor [...]

Ten Daily Electronic Common Sense-Section 4
What are the performances of USB2.0 high-speed OTG?
Compliant USB 2.0 specification OTC; supplementary protocol; running at high speed (480 Mb [...]

Ten Daily Electronic Common Sense-Section 3
What kinds of sensors are used in the electronically controlled suspension system?
Front and rear suspension height sensorBody acceleration se [...]

Ten Daily Electronic Common Sense-Section 2
What is the TA disconnection criterion for line protection?
The difference between the self-produced zero-sequence current and the external ze [...]

Ten Daily Electronic Common Sense-Section 1
Briefly describe the advantages and disadvantages of embedded real-time operating systems?
Develop real-time applications in an embedded real- [...]

Ten Common Sense in Electronics
What is the purpose of the startup code?
The startup code is mostly composed of assembly instructions, which can implement vector table defini [...]

Pitfalls Of Inexpensive Electronic Devices
Many customers choose to buy cheap electronic components for cheap reasons.
However, cheap electronic components mainly have the following defects [...]