1 … 286 287 288 289 290 … 374 2880 / 3740 POSTS

The technical parameters of the А/D converter reflect its performance characteristics. What are the main indicators?

* Question The technical parameters of the А/D converter reflect its performance characteristics. What are the main indicators? * Answer Res [...]

What is the power supply design specification?

* Question What is the power supply design specification? * Answer (1) The full voltage input range is AC90 ~ 265V. (2) The input voltage i [...]

What is the intrinsic photoconductivity effect?

* Question What is the intrinsic photoconductivity effect? * Answer The absorption of light by materials is divided into two types: intrinsi [...]

PCB designers must be creative and learn how to implement those technologies while maintaining those design requirements.

* Question PCB designers must be creative and learn how to implement those technologies while maintaining those design requirements. * Answer [...]

What are the general waveform comparison steps?

* Question What are the general waveform comparison steps? * Answer A general waveform comparison generally requires the following steps: sp [...]

What is the main task of the AFE?

* Question What is the main task of the AFE? * Answer The main task of the AFE is to detect overload and short-circuit faults, and to protec [...]

What are the main types of ARM9 series microprocessors?

* Question What are the main types of ARM9 series microprocessors? * Answer ARM9 series microprocessors mainly include ARM920T, ARM922T and [...]

What are the two types of IC cards?

* Question What are the two types of IC cards? * Answer 1.Contact IC card 2.Contactless IC card [...]

Briefly describe the LT3825/37 pin function?

* Question Briefly describe the LT3825/37 pin function? * Answer (1) SG (1PIN): Secondary side synchronous rectification drive output.The ga [...]

What are the two main methods of suppressing the interference magnetic field?

* Question What are the two main methods of suppressing the interference magnetic field? * Answer 1.Wide range of shielding 2.Gradiometer [...]
1 … 286 287 288 289 290 … 374 2880 / 3740 POSTS