1 … 285 286 287 288 289 … 374 2870 / 3740 POSTS

What is a piezoelectric crystal?

* Question What is a piezoelectric crystal? * Answer There is a very interesting kind of crystal that produces different charges at both end [...]

What are the ways to reduce interrupt latency through software handlers?

* Question What are the ways to reduce interrupt latency through software handlers? * Answer There are two ways to shorten the interrupt lat [...]

What are the types of sensors for electronically controlled in-line pumps?

* Question What are the types of sensors for electronically controlled in-line pumps? * Answer (1) rack position sensor (2) injection adva [...]

Briefly describe the working principle of the DS11-2 elevator load cell?

* Question Briefly describe the working principle of the DS11-2 elevator load cell? * Answer DS11-2 elevator load cell and permanent magnet [...]

What are the inverter operation control functions?

* Question What are the inverter operation control functions? * Answer 1.Starting frequency 2.Adding and decelerating time 3.Jog operati [...]

What points should I pay attention to when using the antenna in the room system?

* Question What points should I pay attention to when using the antenna in the room system? * Answer (1) Try to use a broadband antenna In t [...]

What are the main performance characteristics of TJAl040?

* Question What are the main performance characteristics of TJAl040? * Answer (1) Full compliance with IS011898; (2) High speed (up to 1 M [...]

What is a conductivity type chemical sensor?

* Question What is a conductivity type chemical sensor? * Answer A conductivity type chemical sensor is a measuring device that converts a c [...]

Which types of circuits can be divided into source drive circuits depending on whether a digital-to-analog converter (DAC) is included in the circuit?

* Question Which types of circuits can be divided into source drive circuits depending on whether a digital-to-analog converter (DAC) is included i [...]

What are the advantages of the LIN system?

* Question What are the advantages of the LIN system? * Answer (1) System flexibility (2) Message routing (3) Multicast (4) Bit rate [...]
1 … 285 286 287 288 289 … 374 2870 / 3740 POSTS