1 … 287 288 289 290 291 … 374 2890 / 3740 POSTS

What is an embedded controller?

* Question What is an embedded controller? * Answer The embedded controller eliminates the need for an external PC, making the PXI chassis a [...]

What software is used in the hardware part of the coordinator?

* Question What software is used in the hardware part of the coordinator? * Answer ZigBee wireless module and expansion backplane; the body [...]

Model name of capacitor and method of marking capacitor

* Question Model name of capacitor and method of marking capacitor * Answer The model name of the capacitor is as follows: 1) The model na [...]

What is the application of ZigBee technology?

* Question What is the application of ZigBee technology? * Answer ZigBee technology makes up for the vacancy in the low-cost, low-power and [...]

How is the embedded system composed?What are the characteristics?

* Question How is the embedded system composed?What are the characteristics? * Answer The embedded system consists of embedded microprocesso [...]

What are the applications of automotive sensors?

* Question What are the applications of automotive sensors? * Answer Air flow meter, pressure sensor, position sensor, speed sensor, tempera [...]

Which applications are considered for ZigBee technology?

* Question Which applications are considered for ZigBee technology? * Answer The equipment spacing is small; the equipment cost is very low, [...]

What are the most famous logic synthesis tools in FPGA/CPLD design?

* Question What are the most famous logic synthesis tools in FPGA/CPLD design? * Answer There are three most well-known logic synthesis tool [...]

Several failure modes related to supercapacitors

* Question Several failure modes related to supercapacitors * Answer 1) The well-known bathtub curve reflects early failure and wear failure [...]

What are the currently widely used stochastic mobile models based on independent and identical distribution?

* Question What are the currently widely used stochastic mobile models based on independent and identical distribution? * Answer Random way [...]
1 … 287 288 289 290 291 … 374 2890 / 3740 POSTS