1 … 309 310 311 312 313 … 374 3110 / 3738 POSTS

What is the main function of the constant current circuit?

* Question What is the main function of the constant current circuit? * Answer The constant current circuit has two main functions: inputtin [...]

What are the two main types of oxygen sensors for automobiles?

* Question What are the two main types of oxygen sensors for automobiles? * Answer Oxygen sensors for automobiles mainly include zirconia ty [...]

What is the antenna lobe in the pattern?

* Question What is the antenna lobe in the pattern? * Answer The other lobes of the antenna lobes other than the main lobe are called side l [...]

What constitutes a reader?

* Question What constitutes a reader? * Answer RF signal transmitting unit, high frequency receiving unit and control unit [...]

What are the audio ADC related modules?

* Question What are the audio ADC related modules? * Answer (1) Stereo ADC (2) Audio Recording Selector (3) Recording Gain (4) Automatic [...]

What is the development trend of LED display?

* Question What is the development trend of LED display? * Answer (1) High brightness and full color.Since the advent of blue and pure green [...]

What are the commonly used static calibration devices?

* Question What are the commonly used static calibration devices? * Answer At present, commonly used static calibration devices are: piston [...]

What are the disadvantages of a distributed power system?

* Question What are the disadvantages of a distributed power system? * Answer 1 system design is cumbersome. 2 high cost. [...]

What are the special features of the TV encoder of the S3C6410 processor?

* Question What are the special features of the TV encoder of the S3C6410 processor? * Answer With image enhancement engine, image quality a [...]

What is the role of the Acceptance Filter (ACF)?

* Question What is the role of the Acceptance Filter (ACF)? * Answer The acceptance filter compares the identifier of the received informati [...]
1 … 309 310 311 312 313 … 374 3110 / 3738 POSTS