1 … 311 312 313 314 315 … 374 3130 / 3738 POSTS

What are the two major categories of frequency measurement lines?

* Question What are the two major categories of frequency measurement lines? * Answer One type is to directly read out the frequency value, [...]

What are the challenges that micro thermal management, thermal management and power management products can solve?

* Question What are the challenges that micro thermal management, thermal management and power management products can solve? * Answer Micro [...]

What different bit fields are the data frames composed of?

* Question What different bit fields are the data frames composed of? * Answer (1) Frame start (SOF) (2) Arbitration field (3) Control f [...]

What are the four typical methods of constructing a semiconductor strain gauge?

* Question What are the four typical methods of constructing a semiconductor strain gauge? * Answer Semiconductor strain gauges have the fol [...]

What is magnetic flux?

* Question What is magnetic flux? * Answer The number of lines of magnetic force passing through a cross-sectional area of a magnetic field [...]

What are the cold pressed indium sealing processes?

* Question What are the cold pressed indium sealing processes? * Answer (1) The treatment of the indium sealing surface should be carefully [...]

What is included in the signal channel section?

* Question What is included in the signal channel section? * Answer The input of the measured signal channel 1 and the input of the signal c [...]
DS18B20U+ Temperature Sensor

DS18B20U+ Temperature Sensor

Sensors play a very important role in industrial and consumer electronic equipment. They serve as the eyes and ears of any electronic syst [...]

What is the principle of the 8-digit digital tube?

* Question What is the principle of the 8-digit digital tube? * Answer Each segment of the eight-segment digital display tube is a light-emi [...]

What is the detection method for the outside temperature sensor?

* Question What is the detection method for the outside temperature sensor? * Answer Disconnect the ignition switch and unplug the external [...]
1 … 311 312 313 314 315 … 374 3130 / 3738 POSTS