1 … 307 308 309 310 311 … 374 3090 / 3738 POSTS

What are the main technical features of the TPS7510x?

* Question What are the main technical features of the TPS7510x? * Answer 1 Eliminates the influence of electromagnetic interference (EMI) b [...]

What are the advantages of open-loop non-isolated flyback white LED drivers?

* Question What are the advantages of open-loop non-isolated flyback white LED drivers? * Answer (1) The white LED current can be adjusted w [...]

What are the main components of the DS18B20 internal structure?

* Question What are the main components of the DS18B20 internal structure? * Answer The internal structure of the DS18B20 consists of four m [...]

Brief description of the ISL6754 pin function?

* Question Brief description of the ISL6754 pin function? * Answer (1) VDD: IC power supply terminal.Add a bypass capacitor to GND and a cer [...]

Hard synchronization and resynchronization are two ways of CAN synchronization. What rules do they follow?

* Question Hard synchronization and resynchronization are two ways of CAN synchronization. What rules do they follow? * Answer 1 Only adapt [...]

What kinds of contact torque sensors are there?

* Question What kinds of contact torque sensors are there? * Answer 1.Strain gauge torque sensor 2.Potentiometer type torque sensor [...]

How to configure in FPGA active mode?

* Question How to configure in FPGA active mode? * Answer In the FPGA active mode, the target FPGA actively outputs control and synchronizat [...]

What are the characteristics of the storage device-SD/MMC card host controller?

* Question What are the characteristics of the storage device-SD/MMC card host controller? * Answer Compatible Multimedia Card (MMC) Protoco [...]

Microwave RFID antenna

* Question Microwave RFID antenna * Answer The microwave RFID antenna has various structures and is the main form of the Internet of Things [...]

What are the types of pressure sensors?

* Question What are the types of pressure sensors? * Answer According to the signal principle generated by the sensor, it can be divided int [...]
1 … 307 308 309 310 311 … 374 3090 / 3738 POSTS