1 … 333 334 335 336 337 … 374 3350 / 3738 POSTS

What is the SDA output?

* Question What is the SDA output? * Answer The value of bit 7 to bit 0 (D7 to D0) written in the UiTB register is sequentially output from [...]

What is the reason why the vibrator is selected as a tuning fork type?

* Question What is the reason why the vibrator is selected as a tuning fork type? * Answer Since the two vibrators are moving in the opposit [...]

What is linearity?

* Question What is linearity? * Answer Linearity refers to the degree of linearity between the intensity of the illumination and the resulti [...]

What are the main characteristics of the magnetic triode?

* Question What are the main characteristics of the magnetic triode? * Answer (1) Voltammetric characteristics (2) Magnetoelectric charact [...]

What kinds of security status are there through secure message transmission?

* Question What kinds of security status are there through secure message transmission? * Answer (1) Global security status. (2) Applicatio [...]

What is the structure of the hot wire air flow sensor?

* Question What is the structure of the hot wire air flow sensor? * Answer The hot wire air flow sensor can be divided into two types accord [...]

What are the different requirements for electronic equipment under different system operating conditions?

* Question What are the different requirements for electronic equipment under different system operating conditions? * Answer 1 system can r [...]

What is the role of the Receive Buffer (RxB)?

* Question What is the role of the Receive Buffer (RxB)? * Answer The receive buffer is the interface between the acceptance filter and the [...]

What is a front impact sensor?

* Question What is a front impact sensor? * Answer The front impact sensor is generally mechanical, which is equivalent to a control switch, [...]

What is the basic structure of the FPGA?

* Question What is the basic structure of the FPGA? * Answer Altera's FPGA devices include FLEX10KE, ACEX1K, APEX 20K/20KE, Stratix, Cyclone [...]
1 … 333 334 335 336 337 … 374 3350 / 3738 POSTS