1 … 334 335 336 337 338 … 374 3360 / 3738 POSTS

What are the non-ideal effects in the current mode circuit?

* Question What are the non-ideal effects in the current mode circuit? * Answer The non-ideal effects in the current mode circuit include th [...]

How to apply SJAl000?

* Question How to apply SJAl000? * Answer The register and pin configuration of SJAl000 allows it to use a wide variety of integrated or dis [...]

What are the 32-bit registers accessible to the internal user of the ARM processor?

* Question What are the 32-bit registers accessible to the internal user of the ARM processor? * Answer A total of 37 user-accessible 32-bit [...]

According to whether the IC card and the IC card reader need to be in contact to read and write data, what can the IC card be divided into?

* Question According to whether the IC card and the IC card reader need to be in contact to read and write data, what can the IC card be divided in [...]

What are the characteristics of dual in-line Integrated Circuits(ICs)s?

* Question What are the characteristics of dual in-line Integrated Circuits(ICs)s? * Answer DIP has the following characteristics. (1) It i [...]
What Should We Do If The RTC Clock Has An Occasional Delay Or Timeout?

What Should We Do If The RTC Clock Has An Occasional Delay Or Timeout?

If your RTC clock isn’t giving you same results each time you use it, then there is a possibility of irregular delays or timeouts in the circuit. In a [...]
Five Ways To Protect Against Electrical Power Surges

Five Ways To Protect Against Electrical Power Surges

Electrical power surges definition Electrical power Surge is a voltage spike that is fast, of high rate rise and of a short duration electrical trans [...]
AX88179QF Controller

AX88179QF Controller

Embedded system devices often require a connection with Ethernet. With the advancement in the area of Internet of Things, the demand for E [...]
1N5822RLG Diode

1N5822RLG Diode

Schottky diodes or Schottky rectifiers are solid state electronic components which use metal at the semiconductor junction. These diodes a [...]
TC358743XBG Bridge Device

TC358743XBG Bridge Device

The resolution and the image/video quality of the multimedia content is getting improved by each passing day. This off course means larger [...]
1 … 334 335 336 337 338 … 374 3360 / 3738 POSTS