1 … 341 342 343 344 345 … 374 3430 / 3738 POSTS
NCP1117ST33T3G Regulator

NCP1117ST33T3G Regulator

Almost all modern digital electronic devices require low level DC voltages for their functioning. This low DC voltage allows these electro [...]
LD1117S33TR Regulator

LD1117S33TR Regulator

Almost all modern digital electronic devices require low level DC voltages for their operation. This low DC voltage allows these electroni [...]

What are the commonly used low frequency tags?

* Question What are the commonly used low frequency tags? * Answer Usually, it is a close-range label with a distance of 10 cm or less. It i [...]

What are the functions of the dead zone (DB) module?

* Question What are the functions of the dead zone (DB) module? * Answer Independent ePWMxA input to generate corresponding deadband signal [...]

What are the design of the unit circuit in the digital circuit?

* Question What are the design of the unit circuit in the digital circuit? * Answer 1.Design of combinatorial logic circuit 2.Design of se [...]

What is the working principle of solid state relays?

* Question What is the working principle of solid state relays? * Answer The solid state relay is a kind of four-terminal device with two te [...]

What are the features of the MC9S08DZ60 series?

* Question What are the features of the MC9S08DZ60 series? * Answer (1) 8-bit HCS08 central processing unit (CPU) (2) on-chip memory (3) [...]

What is the working principle of the D/А converter?

* Question What is the working principle of the D/А converter? * Answer The digital quantity of the code is represented by a combination of [...]

What aspects should be considered in the overall design of the automotive electronic control unit?

* Question What aspects should be considered in the overall design of the automotive electronic control unit? * Answer 1 Try to use software [...]

What aspects should be considered in the overall design of the automotive electronic control unit?

* Question What aspects should be considered in the overall design of the automotive electronic control unit? * Answer 1 Try to use software [...]
1 … 341 342 343 344 345 … 374 3430 / 3738 POSTS