1 … 340 341 342 343 344 … 374 3420 / 3738 POSTS

What is the main source of BJT (bipolar triode) noise?

* Question What is the main source of BJT (bipolar triode) noise? * Answer There are three main types of noise in BJT: (1) Thermal noise: [...]

What are the working electrodes and auxiliary electrodes, respectively?

* Question What are the working electrodes and auxiliary electrodes, respectively? * Answer Working electrode and auxiliary electrode Some s [...]

What are the two special features of Rl4 in terms of structure?

* Question What are the two special features of Rl4 in terms of structure? * Answer 1 When a subroutine is called with the BL instruction, t [...]

What are the integrated sensitive units?

* Question What are the integrated sensitive units? * Answer The integrated sensitive unit includes a resilient sensing element and a transd [...]

What is the difference between active and passive drives?

* Question What is the difference between active and passive drives? * Answer the anode and the cathode can emit light, and the driving Ic n [...]

Increase the energy density of EDLC devices.There are three main methods, what are they?

* Question Increase the energy density of EDLC devices.There are three main methods, what are they? * Answer 1 change the electrode material [...]

What are the Virtex class chips?

* Question What are the Virtex class chips? * Answer Current mainstream chips include Vitrex-2, Virtex-2 Pr0, Vitex-4, and Virtex-5. [...]

The reset causes the microcontroller to quickly enter the initial state and execute the program from this state.What are the main effects of reset?

* Question The reset causes the microcontroller to quickly enter the initial state and execute the program from this state.What are the main effect [...]

What are the applications of FPGAs in wireless communication systems?

* Question What are the applications of FPGAs in wireless communication systems? * Answer In terms of data transmission, a large amount of d [...]
NCP1117ST50T3G Regulator

NCP1117ST50T3G Regulator

Almost all modern digital electronic devices require low level DC voltages for their functioning. This low DC voltage allows these electro [...]
1 … 340 341 342 343 344 … 374 3420 / 3738 POSTS