1 … 343 344 345 346 347 … 374 3450 / 3738 POSTS

What are the characteristics of Spartan-3ADSP?

* Question What are the characteristics of Spartan-3ADSP? * Answer Its main features are as follows: 90nm process, density up to 74880 logic [...]

What are the main features of UCC28600?

* Question What are the main features of UCC28600? * Answer (1) Very low standby power consumption (<150mw), in line with Europe's new gr [...]

What are the functions of the AD603 pin?

* Question What are the functions of the AD603 pin? * Answer 1, 2 feet GPOS, GNEG: gain control input (maximum ± 7.5V). 3-pin VINP: Input t [...]

What are the main resource configurations of the OK6410 evaluation board?

* Question What are the main resource configurations of the OK6410 evaluation board? * Answer S3C6410 processor, clocked at 533 MHz/667 MHz; [...]

What is the correspondence between the register organization in the Thumb state and the register organization in the ARM state?

* Question What is the correspondence between the register organization in the Thumb state and the register organization in the ARM state? * An [...]

What is the role of the dual state symbol IO field?

* Question What is the role of the dual state symbol IO field? * Answer The dual state symbol IO field uses a bit variable to switch between [...]

What is the principle of a pyroelectric sensor?

* Question What is the principle of a pyroelectric sensor? * Answer The principle is that spontaneous polarization is generated because the [...]

What are the types of electronic steering system sensors?

* Question What are the types of electronic steering system sensors? * Answer (1) steering wheel angle sensor (2) torque sensor (3) yaw [...]

What are the car manufacturers’ monolithic systems for Nissan?

* Question What are the car manufacturers' monolithic systems for Nissan? * Answer In many Nissan's cars, the power control module has three [...]

What are the navigation system control sensors?

* Question What are the navigation system control sensors? * Answer Car navigation system sensors include geomagnetic sensors (gyro), wheel [...]
1 … 343 344 345 346 347 … 374 3450 / 3738 POSTS