1 … 345 346 347 348 349 … 374 3470 / 3738 POSTS

How to design the hardware system of digital control system?

* Question How to design the hardware system of digital control system? * Answer 1. Determine the overall design plan 2. Identify the syst [...]

What is an organic light emitting diode?

* Question What is an organic light emitting diode? * Answer An organic light emitting diode is a technology that realizes display by using [...]

What are the high power LED constant current drive circuits?

* Question What are the high power LED constant current drive circuits? * Answer (1) AC/DC converter. (2) DC/DC converter. (3) Efficient c [...]

After the control circuit is installed, what items should I check before powering up?

* Question After the control circuit is installed, what items should I check before powering up? * Answer 1.Equipment installation check 2 [...]

What is critical mode work?

* Question What is critical mode work? * Answer The critical mode is a variable-current current-type switching circuit. The external N-chann [...]

What are the three indicators that describe the accuracy of the sensor?

* Question What are the three indicators that describe the accuracy of the sensor? * Answer There are three indicators that show accuracy: p [...]

What is an embedded system?

* Question What is an embedded system? * Answer The embedded system is derived from a microcomputer, and is a computer embedded in an object [...]

What is the static characteristics of the sensor?

* Question What is the static characteristics of the sensor? * Answer When the measured values are in a steady state, the relationship betwe [...]

How are the words and halfwords of the memory defined?

* Question How are the words and halfwords of the memory defined? * Answer The ARM processor directly supports data types of 8-bit bytes, 16 [...]

What are the classifications of the difference in pulse amplitude between various noise pulses and optoelectronic signals?

* Question What are the classifications of the difference in pulse amplitude between various noise pulses and optoelectronic signals? * Answer [...]
1 … 345 346 347 348 349 … 374 3470 / 3738 POSTS