* Question
| Briefly describe the composition and function of the MP 377? |
* Answer
| The MP 370 has a 12″, 15″, 19″ touch screen type, and the 12″ keyboard has 38 system keys and 36 function keys with integrated LEDs.Based on Microsoft Windows CE 5.0, the MP 377 has greatly enhanced its multimedia capabilities compared to the MP 370.The MP 377 has an RS-422/RS-485 interface, two Ethernet interfaces for connection to PROFINET, two USB ports, an MMC slot and a CF card slot, and a two-channel audio output. |

COMMENTS