* Question
| Briefly describe the working principle of the DS11-2 elevator load cell? |
* Answer
| DS11-2 elevator load cell and permanent magnet (round magnet) are used together. When the magnetic field strength at the sensor probe is greater than a certain value, the trigger inside the sensor is turned over, and the output level state of the Hall switch is also followed.Flip, the indicator light is on, output high level signal, otherwise the light is off, |

COMMENTS