* Question Briefly what is WBS? * Answer Work Breakdown Structure (WBS) is the most important tool in project management.…
* Question What are the differences between FPGA and ASIC? * Answer See page 7 Table 1.3
* Question What is information appliance? * Answer What is information appliance?Dr. Vinton Cerf, who invented the Internet TCP/IP standard,…
* Question What are the aspects of embedded Flash programming? * Answer (1) Programmer Programming It is the most primitive…
* Question What are the new and enhanced features of the Cyclone II device family? * Answer Large capacity: Cyclone…
* Question What is a comparison/zero test instruction? * Answer The compare instruction is used to compare the value in…
* Question What is the difference between an inductor and a transformer? * Answer The difference between the inductor and…
* Question What are the functions of the 485BD? * Answer (1) Data transfer without protocol. (2) Data transfer of…
* Question What are the instructions for using the transformer parameters? * Answer (1) When replacing the transformer, it is…
* Question What are the three methods used for the spatial address of the 8051 program memory? * Answer The…