* Question What is the main technology of 0LED? * Answer The new 0LED technology mainly includes phosphorescent OLED, white…
* Question What is a potential type chemical sensor? * Answer A potential type chemical sensor is a measuring device…
* Question What are the characteristics of the Spartan-2 series? * Answer Using 0.18
* Question What are the aspects of compensation for DC bridges? * Answer 1.Zero compensation of DC bridge 2.Temperature drift…
* Question What is the H:X/SP add command? * Answer H: X/SP increment instruction AIX/AIS is used to directly increase…
* Question What is apparent power * Answer In circuits with resistance and reactance, the product of voltage and current…
* Question What is an ATM network? * Answer ATM (Asychronous Transfer Mode) is a high-efficiency, flexible, and novel information…
* Question The networking process is divided into layers that are easier to control and define standard interfaces for interaction…
* Question What should I pay attention to when configuring the FPGA for JTAG? * Answer Make sure all JTAG…
* Question What are the main features of the Enhanced Capture (eCAP) module? * Answer 4 event time stamped register…