• Home
  • QUESTIONS & ANSWERS
  • Power Supplies - Board Mount
  • What conditions must the device meet in order to comply with the PMBus specification?

    * Question

    What conditions must the device meet in order to comply with the PMBus specification?

    * Answer

    The PMBus (Power Management Bus) specification defines a communication protocol and standards for power management devices. To comply with the PMBus specification, a device must meet the following conditions:

    1. Compatibility with SMBus
    – PMBus is built on the System Management Bus (SMBus) protocol, which itself is based on I²C. The device must:
    – Use I²C-compatible hardware for communication.
    – Support SMBus timing and electrical specifications, such as clock speed (typically up to 400 kHz).
    – Support SMBus-specific features like bus arbitration and clock stretching.

    2. Support for PMBus Commands
    – The device must implement PMBus-defined commands and adhere to their functional descriptions. These include:
    – Standard Commands: Such as `READ_VOLTAGE`, `READ_CURRENT`, `WRITE_PROTECTION`.
    – Manufacturer-Specific Commands: Optional commands that extend the functionality while following PMBus rules.
    – It must respond correctly to mandatory commands defined in the PMBus specification.

    3. Addressing
    – Must support 7-bit addressing as specified in SMBus/I²C standards.
    – The device must have a unique address and potentially allow dynamic address assignment if required.

    4. Data Formats
    – Support the specific data encoding formats defined by PMBus, including:
    – Linear Data Format: A two-byte representation for parameters like voltage and current.
    – Direct Data Format: Values directly related to physical quantities.
    – VID Data Format: Voltage Identification encoding for processors.

    5. Timing Requirements
    – Must adhere to SMBus timing specifications for:
    – Clock stretching.
    – Data hold and setup times.
    – Start and stop conditions.

    6. Error Handling
    – Must implement error detection and handling mechanisms, including:
    – PEC (Packet Error Checking): Optional but recommended for ensuring data integrity.
    – Timeout for bus communication as specified in SMBus standards.

    7. Device Capabilities and Identification
    – The device must support commands to query its capabilities, such as:
    – Supported features and command sets.
    – Manufacturer identification via `MFR_ID` and `MFR_MODEL`.

    8. Alert and Fault Handling
    – The device should support PMBus-defined fault handling and reporting mechanisms, such as:
    – Generating alerts for overvoltage, overcurrent, or temperature events.
    – Using the `ALERT` pin for fault reporting, following SMBus alert standards.

    9. Optional Features
    – While not mandatory, the device may support advanced PMBus features, such as:
    – Group command protocols for simultaneous updates.
    – Dynamic bus frequency adjustment.
    – Synchronization with multiple PMBus devices.

    10. Interoperability
    – The device must work seamlessly with other PMBus-compliant devices on the same bus.
    – Ensure backward compatibility with SMBus/I²C to avoid conflicts in mixed environments.

    Summary
    To comply with the PMBus specification, a device must support its communication protocol, timing requirements, data formats, standard commands, and fault/error handling mechanisms. Additionally, it should maintain compatibility with SMBus/I²C and ensure robust and interoperable operation in multi-device environments.