* Question
| What is a carbon film Resistors? The parameters of the carbon film Resistors |
* Answer
| The carbon film Resistors is one of the film Resistorss (FilmResistorss).It uses high-temperature vacuum coating technology to attach carbon to the surface of the ceramic rod to form a carbon film, and then cut it with a suitable joint, and the surface is coated with epoxy resin to protect it.The carbon film Resistors is one of the film Resistorss (FilmResistorss).It uses high-temperature vacuum coating technology to attach carbon to the surface of the ceramic rod to form a carbon film, and then cut it with a suitable joint, and the surface is coated with epoxy resin to protect it. |

COMMENTS