* Question
What is the allowable deviation of the inductor? |
* Answer
The allowable deviation of the inductor indicates the magnitude of the inductance deviation during the manufacturing process, and there are usually l, II, and m levels.The l-level allowable deviation is ±5%, the Il-level allowable deviation is ±10%, and the lIl-level allowable deviation is ±20%.The allowable deviation parameter is not indicated on many smaller inductors |
COMMENTS