• Home
  • QUESTIONS & ANSWERS
  • Others
  • What is the threshold shift phenomenon caused by Joule heat?

    * Question

    What is the threshold shift phenomenon caused by Joule heat?

    * Answer

    The threshold shift phenomenon caused by Joule heat refers to the change in the electrical properties of a semiconductor device, particularly the shift in the threshold voltage (Vth) of transistors such as MOSFETs or other field-effect transistors (FETs), as a result of heat generated by the passage of electric current. This heat is known as Joule heating or self-heating, and it occurs when electrical current passes through a conductor or semiconductor, causing it to resist and dissipate energy as heat.

    Key Points:

    1. Joule Heating in Semiconductors:
    – When a high current flows through the transistor channel, the resistance of the channel causes energy dissipation in the form of heat (Joule heating). As the temperature rises, it can affect the charge carriers and the materials involved, influencing the behavior of the device.

    2. Impact on Threshold Voltage (Vth) :
    – The threshold voltage of a transistor determines the voltage required to turn it on (i.e., to create a conducting channel between source and drain). Under Joule heating, the temperature increase can change the mobility of charge carriers (electrons or holes) and affect the transistor’s material properties.
    – Positive Threshold Shift: The increased temperature often leads to a shift in the threshold voltage, typically increasing it. This means the transistor will require a higher gate voltage to turn on, which can lead to slower switching speeds or failure to operate at low voltages.

    3. Mechanisms of Threshold Shift:
    – Carrier Mobility Degradation: Higher temperatures reduce the mobility of carriers, meaning they move less efficiently through the channel, which increases the threshold voltage.
    – Material Stress and Defects: Prolonged exposure to high temperatures can cause material degradation, such as oxide layer damage in MOSFETs or the introduction of defects, further shifting the threshold voltage.
    – Hot Carrier Injection (HCI): High current densities associated with Joule heating can cause high-energy carriers to become trapped in the gate oxide, contributing to threshold voltage shifts.

    4. Consequences of Threshold Shift:
    – Performance Degradation: The shift in threshold voltage can degrade the performance of the transistor by reducing its current driving capability, increasing leakage current, or causing erratic switching behavior.
    – Device Reliability: Continuous operation under conditions that cause Joule heating can lead to long-term reliability issues such as device failure due to accumulated damage or wear-out mechanisms like electromigration or oxide breakdown.

    This phenomenon is of particular concern in power electronics, where high currents are common, and in scaled-down devices (e.g., in modern microprocessors or mobile devices), where smaller geometries exacerbate the effects of self-heating.

    In summary, the threshold shift phenomenon caused by Joule heat is a critical factor in the reliability and performance of semiconductor devices, particularly in high-power or densely packed electronic circuits.