Ten Daily Electronic Common Sense-Section 78
What are the basic transmission components of PWE3?
User Equipment, Carrier Border Router, Access Link, Pseudo-Wire or Virtual Link, Repeater, [...]

Ten Daily Electronic Common Sense-Section 77
What basic operations will the 28X core perform when executing an instruction?
Fetch instructions from program memory; decode instructions; re [...]

Ten Daily Electronic Common Sense-Section 76
What types of PLC input circuits are usually divided into?
The input circuit of PLC is basically the same, usually divided into 3 types: DC in [...]

Ten Daily Electronic Common Sense-Section 75
What are the main operating frequencies of RFID systems?
Low frequency, 125~l34kHz;High frequency, 13.56MHz;Very high frequency, operating fre [...]

Ten Daily Electronic Common Sense-Section 74
When choosing an IC card adapter, there are several important indicators that cannot be ignored.
Electrical properties of the contacts.The plu [...]

Ten Daily Electronic Common Sense-Section 73
What is hardware reset 1?
Hardware reset 1 is a reset generated through the RESET pin. When the power supply voltage meets the recommended ope [...]

Ten Daily Electronic Common Sense-Section 72
Chip package:
BGA ball grid array packageCSP chip scaling packageChip mounting on COB boardChip Mounting on COC Porcelain SubstrateMCM multi-c [...]

Ten Daily Electronic Common Sense-Section 71
The biggest feature of Modelsim is its powerful debugging features. Which are the main types?
The biggest feature of Modelsim is its powerful [...]

Ten Daily Electronic Common Sense-Section 70
What is the main role of the Event Trigger (ET) module?
Accepts event inputs from the Time Base Counter (TBCTR) and Count Compare (CC) modules [...]

Ten Daily Electronic Common Sense-Section 69
What is COS?
COS (chip operating system) is developed around the characteristics of the smart card it serves.
What are the units of commonl [...]