Ten Daily Electronic Common Sense-Section 38
What is the performance of error detection?
The transmitter can detect all local errors;It has a high error detection rate for the errors of t [...]

Ten Daily Electronic Common Sense-Section 37
What are the common features of PMP currently?
At present, the more common functions of PMP include: MPEG. 4 Play, TV program recording, MP3/W [...]

Ten Daily Electronic Common Sense-Section 36
What types of ARM data processing instructions are there?
Data processing instructions can be roughly divided into three categories: data tran [...]

Ten Daily Electronic Common Sense-Section 35
What are the main performance indicators of the device HA22004P?
Input voltage range: 85~240VAC.Constant current range: 10 ~ 40mA (external ad [...]

Ten Daily Electronic Common Sense-Section 34
What are the main components of the Verilog HDL circuit module?
The general structure of Verilog HDL circuit module mainly includes three part [...]

Ten Daily Electronic Common Sense-Section 33
How does the ARM processor hardware respond to the following process when an abort occurs (assuming the interrupt is not masked)?
When an abno [...]

Ten Daily Electronic Common Sense-Section 32
What are the series of Altera CPLDs?
Altera's CPLDs include MAX 9000, MAX 7000, MAX 3000A and MAX II series.
What is the temperature ri [...]

Ten Daily Electronic Common Sense-Section 31
What functions should the software have for nodes connected to the MOST network?
data transmission control;data message transmission control;p [...]

Ten Daily Electronic Common Sense-Section 30
What are the corresponding functions of the MAC layer?
It can be roughly divided into the following three:Multiple accessResource sharingTrans [...]

Ten Daily Electronic Common Sense-Section 29
What types of counters are there?
Synchronous counterAsynchronous counterImplementation of Arbitrary Base Counter
What conditions must the [...]