1 … 313 314 315 316 317 … 374 3150 / 3738 POSTS

According to the different sensitive membranes, what can ISE be divided into?

* Question According to the different sensitive membranes, what can ISE be divided into? * Answer According to the different sensitive membr [...]

What is the basic principle of DDS?

* Question What is the basic principle of DDS? * Answer The basic principle of DDS is to use the Nyquist time domain sampling theorem to per [...]

What is an embedded system?

* Question What is an embedded system? * Answer According to the IEEE definition, an embedded system is a "device that controls, monitors, o [...]

What is the basic workflow of an RFID system?

* Question What is the basic workflow of an RFID system? * Answer The reader sends a certain frequency of the radio frequency signal. When t [...]

What is the general MFRC500 command?

* Question What is the general MFRC500 command? * Answer (1) The data stream that needs to be input in the command comes directly from the F [...]

What are the common external storage for embedded systems?

* Question What are the common external storage for embedded systems? * Answer Commonly used external storage in embedded systems are: hard [...]

What does the security environment include?

* Question What does the security environment include? * Answer (1) SE identifier (SEID byte) (2) Component (3) Certificate holder's authe [...]

What is the working principle of joint management?

* Question What is the working principle of joint management? * Answer (1) LLC start and stop delay and PGOUT signals (tDELl and toEL2). (2 [...]

What is an RS-485 repeater?

* Question What is an RS-485 repeater? * Answer RS-485 repeaters are required in the following cases: more than 32 stations (including repea [...]

What functions should a hardware of a MOST node have in order to connect to the MOST network?

* Question What functions should a hardware of a MOST node have in order to connect to the MOST network? * Answer (1) clock recovery; (2) [...]
1 … 313 314 315 316 317 … 374 3150 / 3738 POSTS