1 … 312 313 314 315 316 … 374 3140 / 3738 POSTS

What is the output voltage swing?

* Question What is the output voltage swing? * Answer The output voltage swing is the maximum amplitude that the output voltage can achieve [...]

What are the main technical characteristics of the MAXl595 charge pump?

* Question What are the main technical characteristics of the MAXl595 charge pump? * Answer 1) Only three ceramic capacitors are required ex [...]

What is the problem with the probe line?

* Question What is the problem with the probe line? * Answer 1) The public end is suspended.When testing the waveform of the circuit under t [...]

What is the control of high resolution enhanced pulse width modulation?

* Question What is the control of high resolution enhanced pulse width modulation? * Answer Controlled by three 8-bit high resolution regist [...]

What is the composition of the strain strain gauge sensor?

* Question What is the composition of the strain strain gauge sensor? * Answer The resistance strain gauge sensor consists of a spring eleme [...]

Depending on the role of the FPGA in the configuration circuit, how many ways can the configuration data be loaded into the target device?

* Question Depending on the role of the FPGA in the configuration circuit, how many ways can the configuration data be loaded into the target devic [...]

What is an opto-isolator?

* Question What is an opto-isolator? * Answer The photoelectric isolators are isolated from the analog system and the digital system by the [...]

What is an air switch

* Question What is an air switch * Answer Automatic air switches, also known as low-voltage circuit breakers, can be used to switch the load [...]

What are the commonly used random access memories?

* Question What are the commonly used random access memories? * Answer (1) Static RAM (SRAM) Static RAM is characterized by the ability to r [...]

What are the microprocessor units included?

* Question What are the microprocessor units included? * Answer The microprocessor unit includes digital memory (EEPROM, ROM, RAM), an I/O i [...]
1 … 312 313 314 315 316 … 374 3140 / 3738 POSTS