1 … 316 317 318 319 320 … 374 3180 / 3738 POSTS

What are the main technical features of the MAX6966?

* Question What are the main technical features of the MAX6966? * Answer 1 with high-speed 26MHz SPI / QSPI / MICROWIRE compatible serial po [...]

How to design a fast data exchange mechanism for multi-DSP digital controllers?

* Question How to design a fast data exchange mechanism for multi-DSP digital controllers? * Answer Commonly used implementation methods are [...]

What functions are completed by the substation inspection system based on sensor technology and RFID radio frequency identification technology?

* Question What functions are completed by the substation inspection system based on sensor technology and RFID radio frequency identification tech [...]

What is the role of Error Management Logic (EML)?

* Question What is the role of Error Management Logic (EML)? * Answer The error management logic completes the error handling of the transpo [...]

What are the TV encoder related registers?

* Question What are the TV encoder related registers? * Answer 1. TV Controller control SFR set 2. Vertical back porch end point 3. Hori [...]

What are the CAN test content?

* Question What are the CAN test content? * Answer (1) CAN bus test is generally divided into two parts: single node test and bus system int [...]

What are the characteristics of three-phase sinusoidal AC?

* Question What are the characteristics of three-phase sinusoidal AC? * Answer (1) The frequency of each phase of sinusoidal alternating cur [...]

What is a discrete solution?

* Question What is a discrete solution? * Answer The discrete solution is a power management system implemented by a discrete IC that limits [...]

What is a safety sensor?

* Question What is a safety sensor? * Answer Safety sensors, also known as guard sensors, are primarily used to prevent accidental detonatio [...]

If the ADC and DAC are enabled and powered up before the sample rate is changed, the sample rate value change will be valid, so how is the sample rate set?

* Question If the ADC and DAC are enabled and powered up before the sample rate is changed, the sample rate value change will be valid, so how is t [...]
1 … 316 317 318 319 320 … 374 3180 / 3738 POSTS