1 … 314 315 316 317 318 … 374 3160 / 3738 POSTS

Altera Cyclone FPGAs have the following performance characteristics?

* Question Altera Cyclone FPGAs have the following performance characteristics? * Answer New programmable architecture for low cost design.E [...]

What is the thermoelectric effect?

* Question What is the thermoelectric effect? * Answer The thermoelectron effect is also caused by an increase in electric field strength du [...]

What are the reasons for the change in strain gauge resistance due to changes in ambient temperature?

* Question What are the reasons for the change in strain gauge resistance due to changes in ambient temperature? * Answer There are two reas [...]

What is the basic workflow of an RFID system?

* Question What is the basic workflow of an RFID system? * Answer The reader sends a certain frequency of the radio frequency signal. When t [...]

What is the detection limit?

* Question What is the detection limit? * Answer Detection limit: The lowest concentration at which ISE can detect ions. [...]

What are the car manufacturers’ general-purpose single-chip systems for general-purpose vehicles?

* Question What are the car manufacturers' general-purpose single-chip systems for general-purpose vehicles? * Answer Many GM's power contro [...]

4500 series chip function

* Question 4500 series chip function * Answer Model device name Remarks CD45014 input double AND gate and 2 input or non-gate CD4502 optiona [...]

What are the characteristics of photoelectric switches?

* Question What are the characteristics of photoelectric switches? * Answer Photoelectric switches are characterized by small size, high spe [...]
19-217/Y5C-AM1N1VY/3T Chip LED

19-217/Y5C-AM1N1VY/3T Chip LED

The development of LED (light emitting diode) is regarded as one of the greatest milestones in the history of semiconductor and electronic [...]

How to easily identify common varactor diodes?

* Question How to easily identify common varactor diodes? * Answer The varactor diode is a special diode specially designed according to the [...]
1 … 314 315 316 317 318 … 374 3160 / 3738 POSTS