1 … 315 316 317 318 319 … 374 3170 / 3738 POSTS

What are the three ways to self-test?

* Question What are the three ways to self-test? * Answer (1) Power-on self-test (2) Periodic self-test (3) Key-controlled self-test [...]

What are the advantages of the Virtex-6 FPGA family?

* Question What are the advantages of the Virtex-6 FPGA family? * Answer The advantages of the Virtex-6 FPGA family are as follows: (1) Easi [...]

What is a three-terminal adjustable negative power regulator?

* Question What is a three-terminal adjustable negative power regulator? * Answer The three-terminal adjustable negative power regulator com [...]

If the ADC and DAC are enabled and powered up before the sample rate is changed, the sample rate value change will be valid, so how is the sample rate set?

* Question If the ADC and DAC are enabled and powered up before the sample rate is changed, the sample rate value change will be valid, so how is t [...]

What is the way to detect roads?

* Question What is the way to detect roads? * Answer 1 Turn on the ignition switch, do not start the engine, check the ECU connector B termi [...]

What is a safety sensor?

* Question What is a safety sensor? * Answer Safety sensors, also known as guard sensors, are primarily used to prevent accidental detonatio [...]

What is a discrete solution?

* Question What is a discrete solution? * Answer The discrete solution is a power management system implemented by a discrete IC that limits [...]

What are the characteristics of three-phase sinusoidal AC?

* Question What are the characteristics of three-phase sinusoidal AC? * Answer (1) The frequency of each phase of sinusoidal alternating cur [...]

What are the performance and features of Microchip’s digital controller solutions?

* Question What are the performance and features of Microchip's digital controller solutions? * Answer 1 Increased power density. 2 lower c [...]

The amount of information transmitted by the tag also directly affects the polling time.Therefore, what are the main considerations for achieving time validity?

* Question The amount of information transmitted by the tag also directly affects the polling time.Therefore, what are the main considerations for [...]
1 … 315 316 317 318 319 … 374 3170 / 3738 POSTS