1 … 318 319 320 321 322 … 374 3200 / 3738 POSTS

What are the main technical features of the MAX6966?

* Question What are the main technical features of the MAX6966? * Answer 1 with high-speed 26MHz SPI / QSPI / MICROWIRE compatible serial po [...]

The amount of information transmitted by the tag also directly affects the polling time.Therefore, what are the main considerations for achieving time validity?

* Question The amount of information transmitted by the tag also directly affects the polling time.Therefore, what are the main considerations for [...]

How to easily identify common varactor diodes?

* Question How to easily identify common varactor diodes? * Answer The varactor diode is a special diode specially designed according to the [...]
LTST-C190GKT SMD LED

LTST-C190GKT SMD LED

The invention of LED (light emitting diode) is considered as one of the biggest milestones in semiconductor and electronics technology. Be [...]
CAT24C32WI-GT3 EEPROM

CAT24C32WI-GT3 EEPROM

In the past few decades, the electronics technology has seen unprecedented growth and advancement. From rudimentary analog devices of the [...]

What are the three major categories of electrolytes for electric double layer capacitors?

* Question What are the three major categories of electrolytes for electric double layer capacitors? * Answer 1 water system; 2 salt disso [...]

Which two types of sensors are calibrated?

* Question Which two types of sensors are calibrated? * Answer The calibration of the sensor is divided into static calibration and dynamic [...]

What are the main technical features of the MAX7316?

* Question What are the main technical features of the MAX7316? * Answer 1400kbit/s, 2-wire serial interface, 5.5V voltage tolerance; 2 wor [...]

What is a CRC operation?

* Question What is a CRC operation? * Answer The CRC (Cyclic Redundancy Check) operation detects an error in the data block.The microcontrol [...]

What are the main technical indicators of stepper motors?

* Question What are the main technical indicators of stepper motors? * Answer 1. Working voltage, 2. Winding current 3. Torque torque 4. [...]
1 … 318 319 320 321 322 … 374 3200 / 3738 POSTS