1 … 338 339 340 341 342 … 374 3400 / 3738 POSTS

What is the main source of BJT (bipolar triode) noise?

* Question What is the main source of BJT (bipolar triode) noise? * Answer There are three main types of noise in BJT: (1) Thermal noise: [...]

What is a central collision sensor?

* Question What is a central collision sensor? * Answer The central impact sensor, also known as the central acceleration sensor, detects th [...]

What is the branch current method?

* Question What is the branch current method? * Answer A circuit that cannot be equivalent to a Resistors-parallel equivalent conversion is [...]

What is the detection method of the switch contact throttle position sensor?

* Question What is the detection method of the switch contact throttle position sensor? * Answer 1 general inspection. 2 open circuit detec [...]

What are the integrated sensitive units?

* Question What are the integrated sensitive units? * Answer The integrated sensitive unit includes a resilient sensing element and a transd [...]

What is the difference between active and passive drives?

* Question What is the difference between active and passive drives? * Answer 1.Different Structures The pixels of the passive drive matrix [...]

Increase the energy density of EDLC devices.There are three main methods, what are they?

* Question Increase the energy density of EDLC devices.There are three main methods, what are they? * Answer 1 change the electrode material [...]

What are the Virtex class chips?

* Question What are the Virtex class chips? * Answer Current mainstream chips include Vitrex-2, Virtex-2 Pr0, Vitex-4, and Virtex-5. [...]

The reset causes the microcontroller to quickly enter the initial state and execute the program from this state.What are the main effects of reset?

* Question The reset causes the microcontroller to quickly enter the initial state and execute the program from this state.What are the main effect [...]

What are the applications of FPGAs in wireless communication systems?

* Question What are the applications of FPGAs in wireless communication systems? * Answer In terms of data transmission, a large amount of d [...]
1 … 338 339 340 341 342 … 374 3400 / 3738 POSTS