* Question
What are the fundamental principles for dividing software functional modules in numerical control (NC) systems?
* Answer
Software design for numerical control (NC/CNC) systems typically adopts a modular architecture to ensure reliability, real-time performance, and ease of maintenance. When dividing functional modules, engineers follow several core principles to achieve a clean, scalable, and high-performance system.
1. Single Responsibility Principle (SRP)
Each module should be responsible for one clearly defined function only.
Examples:
- Interpolation module
- Servo control module
- Human–machine interface (HMI) module
This reduces complexity and makes testing, debugging, and maintenance more efficient.
2. High Cohesion
Functions that are closely related should be grouped into the same module.
High cohesion ensures that:
- Module logic is focused
- Internal interactions are efficient
- Code readability and reliability improve
For example, all motion-planning algorithms belong in one cohesive planning module.
3. Low Coupling
Modules should minimize dependencies on each other.
Benefits include:
- Lower impact of changes
- Easier module replacement or upgrading
- Higher system flexibility
NC systems often separate:
- Motion control
- I/O management
- Error handling
- Communication interfaces
to reduce interdependencies.
4. Clear Interfaces and Standardized Communication
Modules interact through well-defined, standardized interfaces:
- API calls
- Task/event messaging
- Data buffers
- Shared memory with strict access rules
This prevents hidden dependencies and allows easier integration and expansion.
5. Real-Time Requirements
NC software includes hard real-time components (e.g., servo loops, interpolation) and non-real-time components (e.g., UI).
Module division must reflect timing constraints:
- Real-time tasks separated into dedicated modules
- Non-real-time tasks isolated to avoid interference
- Priority scheduling clearly partitioned
This ensures deterministic system behavior.
6. Functional Independence and Replaceability
Modules should be designed so that they can be independently modified, upgraded, or replaced without affecting the rest of the system.
Example: Replacing a communication protocol module (RS232 → Ethernet) should not impact the motion control module.
7. Scalability and Extensibility
Module division must consider:
- Multi-axis expansion
- New machining processes
- Future hardware upgrades
- Optional advanced functions (e.g., 5-axis interpolation, adaptive feed control)
Good modularity ensures the system can evolve without major redesign.
8. Error Isolation and Fault Tolerance
Modules should isolate faults so that an error in one module does not cause system-wide failures.
Examples:
- Independent error-handling module
- Separate diagnostic and logging module
This improves safety and reliability in industrial environments.
Summary
When dividing functional modules in NC software design, engineers follow principles including single responsibility, high cohesion, low coupling, clear interfaces, real-time partitioning, independence, scalability, and robust error isolation. These principles together ensure that numerical control systems remain reliable, maintainable, and adaptable to future technological requirements.

COMMENTS