• Home
  • QUESTIONS & ANSWERS
  • Others
  • What Are the Units of Commonly Used Resistors?

    * Question

    What Are the Units of Commonly Used Resistors?

    * Answer

    The value of a resistor indicates how much it resists the flow of electric current.
    This resistance is measured using standard units defined by the International System of Units (SI).

    The commonly used units for resistors are based on the ohm (Ω).

    1. Ohm (Ω)

    The ohm (Ω) is the basic unit of resistance.

    • 1 Ω means the resistance that allows 1 ampere of current to flow when 1 volt is applied
    • Used for low-resistance components

    Typical examples:

    • 10 Ω
    • 220 Ω
    • 1 kΩ (1000 Ω)

    2. Kilohm (kΩ)

    The kilohm (kΩ) is equal to 1,000 ohms.

    1 kΩ=1,000Ω

    Typical applications:

    • Signal circuits
    • Pull-up or pull-down resistors
    • Bias networks

    Common values:

    • 7 kΩ
    • 10 kΩ
    • 47 kΩ

    3. Megohm (MΩ)

    The megohm (MΩ) is equal to 1,000,000 ohms.

    1 MΩ=1,000,000Ω

    Typical applications:

    • High-impedance circuits
    • Voltage measurement and sensing
    • Leakage current limiting

    Common values:

    • 1 MΩ
    • 10 MΩ

    4. Sub-Ohm Units (Milliohm, mΩ)

    For very low resistance values, milliohms (mΩ) are used.

    1 mΩ=0.001Ω

    Typical applications:

    • Current sensing resistors
    • Power management circuits

    These resistors are designed for high-current measurement.

    Engineering Insight

    Resistor values are often printed using:

    • Color codes
    • Numeric markings
    • EIA codes (for SMD resistors)

    Understanding resistance units helps customers:

    • Read resistor values correctly
    • Select proper components
    • Avoid wiring and design errors

    Conclusion

    The commonly used units for resistors are:

    • Ohm (Ω)– basic unit
    • Kilohm (kΩ)– thousands of ohms
    • Megohm (MΩ)– millions of ohms
    • Milliohm (mΩ)– very low resistance values

    These units cover the full range of resistor applications, from high-current sensing to high-impedance signal control.

    COMMENTS

    WORDPRESS: 0
    DISQUS: 0