Solid State Relays: Types, Selection Criteria, and Sourcing Discontinued Models

  • Home
  • SUPPLY CHAIN INSIGHTS
  • Solid State Relays: Types, Selection Criteria, and Sourcing Discontinued Models

    Solid state relays (SSRs) are a mature but continually relevant switching technology, found in everything from industrial heating systems and PLC-controlled machinery to medical devices and renewable energy equipment. Unlike their electromechanical counterparts, SSRs perform all switching through semiconductor junctions, with no mechanical contacts involved. That single architectural difference has broad downstream consequences — for performance, lifespan, thermal behavior, and ultimately for how you source and manage them across a product’s lifecycle.

    This article covers the principal types of solid state relays, what differentiates them at a technical level, the selection parameters that matter most in practice, and the specific challenges engineers and procurement teams face when an SSR family reaches end-of-life or is discontinued by its original manufacturer.

    Technical Guide
    Solid State Relays

    Types, Selection Criteria & Sourcing Discontinued Models — a visual summary

    What Is a Solid State Relay?

    An SSR is an electronic switch using semiconductor junctions (thyristors, triacs, MOSFETs) instead of mechanical contacts. Control and load circuits are optically isolated — no moving parts, no arcing, no electromagnetic noise.

    0
    Moving Parts
    Millions
    Cycles, No Wear
    µs
    Switching Speed
    ~1.2 W/A
    Heat per Amp Switched
    4 Output Technology Types
    ⚡
    Triac-Based

    Dominant for AC loads — heaters, lamps. Zero-crossing versions cut EMI. Not for DC.

    SCR Back-to-Back

    Dual SCRs in antiparallel. Handles high-surge AC industrial loads more robustly.

    MOSFET-Based

    Preferred for DC switching. Low leakage, fast transitions. Common in embedded & battery systems.

    PhotoMOS

    Small-signal. Ideal for test equipment & instrumentation. Zero bounce, high signal integrity.

    Switching Modes for AC SSRs
    Zero-Crossing

    Turns on at voltage zero. Minimizes inrush & EMI. Best for resistive loads & noise-sensitive environments.

    Instant-On

    Energizes immediately on signal, regardless of waveform phase. Right for inductive loads & timing-critical apps.

    Peak-Switching

    Turns on at AC voltage peak. Suited for heavy inductive loads requiring maximum voltage at turn-on.

    Key Selection Parameters
    Load Type & Current

    AC or DC? Resistive, inductive, or capacitive? Size to ~⅔ rated current for resistive loads. Derate to ⅕–⅐ for inductive/capacitive.

    Control Signal

    Match pick-up/drop-out voltages to PLC, MCU GPIO, or controller output. Common range: 3–32V DC logic-level.

    Isolation Voltage

    Confirm input-output isolation is adequate. Critical for safety in high-voltage industrial or medical applications.

    Thermal Design

    SSRs generate ~1.2 W per amp. Use derating curves. Panel-mount units require proper heatsink + thermal compound.

    Mounting Style

    PCB for board-level low/med power. Panel for heatsink-attached chassis. DIN rail for industrial panels with integrated heatsink.

    ⚙️
    Switching Mode

    Zero-crossing = default for resistive & EMI-sensitive. Instant-on = inductive or timing-critical. Peak = heavy inductive.

    SSR vs Electromechanical Relay
    ✅ SSR Advantages
    • No moving parts — no wear, bounce, or arcing
    • Microsecond switching speed
    • Millions of cycles with no degradation
    • Silent operation — no audible click
    • No EMI from switching coil
    ⚠️ SSR Tradeoffs
    • Higher heat generation per unit current
    • Requires dedicated thermal management
    • Typically single-output contact only
    • Higher unit cost than EMR
    • Not ideal for multi-pole configurations
    Sourcing Discontinued SSRs: 3 Paths
    1
    Last-Time Buy (LTB)

    Purchase stock before EOL closes. Viable only with 6–12 months’ notice and reliable demand forecasts to avoid excess inventory.

    2
    Functional Equivalent

    Match critical parameters: output voltage, current, control voltage, switching mode, isolation & footprint. Engineering validation still required.

    3
    Alternative Solution

    No drop-in exists? Consider form-factor change (panel → DIN rail) or circuit redesign. Work with a specialist distributor for guidance.

    Proactive Lifecycle Risk Checklist
    ✓

    Monitor lifecycle status — subscribe to manufacturer EOL/PCN notifications for all active BOM parts

    ✓

    Audit BOM for single-sourced SSRs — flag any design dependent on one manufacturer or one part number

    ✓

    Pre-qualify functional equivalents — identify approved alternates before an EOL event forces the issue

    ✓

    Build strategic inventory — for parts with long requalification times or high replacement costs

    ✓

    Engage a lifecycle sourcing partner — engage an independent distributor with an obsolescence programme as a standing resource, not at the crunch

    Key Takeaway

    SSR selection is a multi-dimensional exercise: output technology, switching mode, electrical derating, and thermal design all determine whether a design succeeds in the field. Lifecycle management is an equally important — and often overlooked — engineering variable. The teams that manage it best monitor proactively, pre-qualify alternates early, and partner with sourcing specialists long before a shortage or EOL event forces their hand.

    Need to Source a Discontinued or Hard-to-Find SSR?

    WIN SOURCE is a global independent distributor of electronic components, supporting component supply, shortage sourcing, lifecycle management and alternative solutions.

    Submit an RFQ →

    WIN SOURCE · Global Independent Electronic Components Distributor

    AS9120ISO 9001ISO 14001ERAI Member

    What Is a Solid State Relay?

    A solid state relay is an electronic switching device that uses semiconductor components — thyristors, triacs, transistors, or MOSFETs — to open and close a circuit in response to a low-level control signal, without any physical contacts making or breaking the connection. The control and load circuits are electrically isolated, typically by an optocoupler or transformer, which means a microcontroller or PLC output can safely switch a high-voltage AC or DC load with no direct electrical path between the two sides of the circuit.

    The internal architecture varies by output type, but the basic function is consistent: apply a signal within the input voltage range, and the semiconductor switch conducts; remove it, and the device returns to a non-conducting state. Because there are no moving parts to wear out, no contacts to arc, and no coil to generate electromagnetic noise, SSRs behave very differently from traditional relays under repeated operation.

    SSR vs. Electromechanical Relay: When Each Makes Sense

    Electromechanical relays (EMRs) remain the practical choice for certain applications — particularly low-duty-cycle switching, multi-pole configurations, or situations where initial cost is the dominant constraint. However, in applications involving high cycle rates, noise-sensitive environments, or demanding mechanical conditions, SSRs offer clear advantages that often outweigh their higher unit cost.

    SSRs have no moving parts, which eliminates contact bounce, arcing, and mechanical wear as failure modes. In terms of operational longevity, SSRs can run for millions of cycles with no measurable degradation in performance, well beyond what a mechanical contact set achieves before its contacts erode. Switching speed is another differentiator: SSRs transition in microseconds using semiconductor junctions, while EMRs are constrained by the physical inertia of their mechanical contacts, operating on the order of milliseconds. For applications near PLCs, HMIs, or other sensitive control electronics, the absence of switching noise and audible click is also a meaningful practical benefit.

    The tradeoffs are real. SSRs generate more heat per unit current than EMRs due to their on-state forward voltage drop, which means thermal management is a design requirement, not an afterthought. They also typically offer only a single output contact, limiting their use in applications that need multi-pole switching in a single package. Knowing these tradeoffs is the starting point for any SSR selection process.

    Types of Solid State Relays

    SSRs are not a monolithic category. They differ across four meaningful dimensions: output technology, switching mode, contact configuration, and physical mounting style. Each dimension affects performance characteristics and application fit.

    By Output Technology

    The output stage defines what kind of load an SSR can drive reliably, and choosing the wrong technology is one of the most common application errors.

    • Triac-based SSRs are the dominant choice for AC load control — heaters, lamps, and general line-frequency AC equipment. They are a mature, well-understood solution, and zero-crossing versions reduce electromagnetic interference significantly. However, triacs are not suited for DC loads, have a holding current requirement, and can behave unpredictably with very light or highly reactive loads.
    • SCR (thyristor) back-to-back SSRs use two silicon-controlled rectifiers arranged in antiparallel, providing a more robust alternative to triacs for demanding AC industrial environments with high surge currents or harsh electrical conditions. This configuration handles high-cycle heater control and heavy industrial loads more reliably than a single triac.
    • MOSFET-based SSRs are preferred for DC load switching. They offer low control power requirements, typically lower leakage current than AC triac types, and fast turn-on and turn-off. The on-resistance (RON) of the MOSFET generates heat proportional to load current, so current capability and thermal design matter. This type is common in embedded systems, battery-powered equipment, and DC motor control.
    • PhotoMOS (MOSFET optocoupler) relays are small-signal SSRs used primarily in test equipment, instrumentation, and analog signal switching. They have no contact bounce and long operational life, making them useful where signal integrity and repeatability matter more than high current capacity.

    By Switching Mode

    For AC-output SSRs, the point in the AC cycle at which the device turns on has application-specific implications.

    • Zero-crossing (zero-voltage switching) SSRs wait until the AC load voltage passes through zero before turning the output on. This minimizes inrush current and suppresses conducted EMI, making zero-crossing types the standard choice for resistive loads such as heaters and incandescent lamps, as well as for applications near sensitive digital control systems.
    • Instant-on (random turn-on) SSRs energize the output immediately when the control signal is applied, regardless of where the AC waveform is in its cycle. This mode is appropriate for inductive loads and applications where precise timing relative to the control signal matters more than minimizing switching transients.
    • Peak-switching SSRs turn on when the control signal is present and the AC voltage reaches its peak. This mode is specifically suited to heavy inductive loads where maximum voltage at turn-on helps establish current flow more cleanly.

    By Contact Configuration

    SSR switch configurations parallel the standard relay form factor terminology. Form A devices are single-pole, single-throw and normally open — the most common configuration, used whenever the SSR simply needs to turn a load on and off. Form B devices are also SPST but normally closed, used where the default state requires current flow that stops when the control signal is applied. Form C devices are single-pole, double-throw changeover switches, offering both normally open and normally closed contacts in a single package, though these are less common in SSR implementations than in electromechanical relays.

    By Mounting Style

    Physical packaging determines how an SSR integrates into a system and directly affects its thermal management options.

    • PCB mount SSRs are designed for through-hole or surface-mount installation on a printed circuit board. They are used in low-to-medium power applications where space is constrained and switching takes place close to other board-level components.
    • Panel mount SSRs are intended for direct attachment to a chassis or heatsink plate. At higher load currents, panel mount types must be mounted to a properly sized metal heatsink — operating them without one at rated current will cause thermal failure.
    • DIN rail mount SSRs integrate directly into industrial control panels using standard rail hardware. Many DIN rail models include an integrated heatsink, simplifying thermal design and installation, and some snap directly onto the rail without additional hardware.

    Key Selection Parameters

    Selecting an SSR requires matching several electrical and environmental parameters to the specific application. Treating any one of them as secondary tends to cause field failures.

    Load type and output voltage/current are the primary starting point. Determine whether the load is AC or DC, resistive, inductive, or capacitive, and establish the normal operating current and the expected surge or inrush current. The general guidance is to size SSRs conservatively: operating at roughly two-thirds of rated current for resistive loads improves reliability and thermal behavior, while inductive or capacitive loads may require derating the SSR to one-fifth or one-seventh of its current rating to survive inrush conditions safely.

    Control signal compatibility is the next check. SSRs are available with logic-level DC inputs (3–32V DC is a common range), AC control inputs, and higher-voltage DC inputs. The SSR’s specified pick-up and drop-out voltages must be matched to the output of the control circuit — PLC output card, microcontroller GPIO, temperature controller, or other source — with appropriate margin at both ends of the voltage range.

    Switching mode should be chosen based on load type and EMI sensitivity. Zero-crossing types are the default for resistive loads in electrically noisy environments; random turn-on types are appropriate for inductive or timing-critical loads.

    Isolation voltage and form factor complete the selection checklist. Confirm that the input-output isolation voltage is adequate for the application, and choose the mounting style based on the physical installation context (PCB, panel, or DIN rail) and the thermal management approach available.

    Thermal Management Considerations

    Thermal performance is the most common source of SSR field failures and is often underestimated during design. Every SSR generates heat as a result of the forward voltage drop across its output semiconductor junction — at a rate of roughly 1.2 W per amp of load current for a typical AC output stage. How much temperature rise that produces depends on the thermal resistance of the heatsink and the ambient conditions, so this self-heating limits the current that can be sustained at a given ambient temperature, and SSR datasheets typically include derating curves that show how rated current must be reduced as temperature rises.

    Panel mount SSRs must be installed on a properly prepared metal heatsink with thermally conductive compound applied to the interface surface. Vertical orientation aids passive convection, and the heatsink must be sized for the actual load current and ambient temperature — not just the SSR’s nominal rating. DIN rail-mounted SSRs with integrated heatsinks simplify this step but still require adequate airflow within the enclosure. Operating any power-rated SSR without proper heatsinking under load will result in thermal runaway and device failure.

    SSRs with integrated thermal protection — built-in thermostats or temperature-sensing shutdown circuits — add a layer of protection against unexpected thermal conditions, though these features do not substitute for proper system-level thermal design. For high-current applications or dense panel layouts, forced-air cooling should be considered alongside passive heatsinking.

    Sourcing Discontinued and End-of-Life SSR Models

    SSR product families have finite commercial lives, and discontinuation events are neither rare nor predictable. Upstream supply constraints can pull a manufacturer’s EOL timeline forward, and an entire family can be withdrawn rather than a single part number. When a specific SSR part number that is embedded in a fielded product or production line goes end-of-life, the options available depend heavily on how early the signal was detected.

    The three practical paths when a required SSR model is discontinued are last-time buys, functional equivalents, and alternative solutions:

    • Last-time buys (LTB) involve purchasing sufficient stock before the manufacturer formally closes out the part. This is only viable when the EOL notice is received early enough — typically six to twelve months before the end-of-sale date — and when demand forecasts are reliable enough to justify the inventory investment without creating excess stock that ties up capital.
    • Functional equivalents are current-production parts from the same or a different manufacturer that match the critical electrical parameters: output voltage range, load current rating, input control voltage, switching mode, isolation voltage, and package footprint. In some cases, manufacturers publish transition tools that map obsolete part numbers to recommended replacements, though these do not always exist, and final approval of any substitution belongs to the customer’s engineering team — a parameter match is necessary but not sufficient.
    • Alternative solutions address cases where neither an exact nor a pin-compatible replacement exists. This may involve a form factor change — for example, moving from a panel-mount to a DIN rail design with equivalent electrical characteristics — or a circuit-level redesign. An experienced component distributor with technical depth can accelerate this process by providing application-level guidance alongside potential replacement candidates.

    Finding genuine stock of a discontinued SSR model means working with suppliers that hold inventory beyond the original production run and can document where it came from. WIN SOURCE is a global independent distributor of electronic components, supporting component supply, shortage sourcing, lifecycle management and alternative solutions across product categories including solid state relays — current-production models as well as parts that are hard to find — with verified stock and cross-reference support.

    Building Proactive Supply Chain Resilience for SSRs

    The most effective approach to SSR lifecycle risk is not reactive sourcing after a discontinuation notice — it is proactive monitoring and relationship management before that notice arrives. Product lifecycles for electronic components, including SSRs, follow recognizable patterns, and parts with narrow sourcing bases, aging semiconductor processes, or declining sales volumes are statistically more likely to face EOL actions.

    A structured approach to component lifecycle management covers several dimensions: monitoring manufacturer lifecycle status notifications for parts in active use, maintaining BOM-level visibility into which production designs rely on single-sourced SSRs, identifying functional equivalents before they are needed, and maintaining strategic inventory for parts with long replacement lead times or high requalification costs. Supply chain specialists at both the internal engineering level and the distributor level play a role in this process — the earlier a potential obsolescence event is identified, the more options remain available and the lower the risk premium on sourcing.

    For organizations managing large or complex BOMs, tools that automate lifecycle status tracking and flag approaching end-of-sale dates can significantly reduce the exposure to emergency sourcing situations. WIN SOURCE is built to be engaged as a long-term supply chain resource across a component’s full commercial life rather than only at the point of shortage, with cost control management, BOM analysis and procurement support alongside day-to-day component supply.

    Summary

    Solid state relays cover a broader design space than their single-category name suggests. Output technology (triac, SCR, MOSFET, PhotoMOS), switching mode (zero-crossing, instant-on, peak), contact form, and mounting style each contribute to whether a given SSR will perform reliably in a specific application. Selection requires matching electrical parameters — load voltage, current, control signal, isolation — with sufficient derating margin, and it requires a thermal design that accounts for the SSR’s inherent self-heating under load.

    Beyond the application design phase, the commercial lifecycle of an SSR model is a separate engineering and procurement variable. Discontinuation events are common across the industry, driven by upstream supply constraints, process changes, and market evolution. The teams that manage this risk most effectively are those that monitor component lifecycle status continuously, identify alternatives before they are needed, and work with sourcing partners who can support both in-production procurement and end-of-life inventory access across the full lifecycle of a product design.

    Frequently Asked Questions

    What is the difference between a solid state relay and an electromechanical relay?

    An SSR switches through semiconductor junctions with no moving parts, so there is no contact bounce, no arcing and no audible click, and it switches in microseconds rather than milliseconds. An electromechanical relay is still the practical answer for low-duty-cycle switching, multi-pole configurations, and designs where unit cost dominates — and it runs cooler, because an SSR dissipates real power across its output stage whenever it conducts.

    How much should I derate a solid state relay?

    For a resistive load, sizing the SSR at roughly two-thirds of its rated current is a common starting point. Inductive and capacitive loads draw large inrush currents, and there the usual guidance is far more conservative — on the order of a fifth to a seventh of the rating. Work from the datasheet’s own derating curves at your actual ambient temperature rather than from the headline current figure.

    Do solid state relays need a heatsink?

    Any power-rated SSR carrying meaningful current does. The output stage dissipates roughly 1.2 W per amp of load current, and the temperature that produces depends entirely on the thermal path away from the device. Panel-mount units need a correctly sized metal heatsink with thermal compound at the interface; DIN-rail units often integrate one but still need airflow in the enclosure.

    Which SSR output technology should I use for a DC load?

    A MOSFET-based SSR. Triacs and back-to-back SCRs need the AC waveform to cross zero in order to turn off, so they cannot reliably interrupt a DC load. MOSFET types also offer low control power, low leakage and fast transitions, which is why they dominate embedded, battery-powered and DC motor control applications.

    What are my options when an SSR model is discontinued?

    A last-time buy while the part is still orderable, a functional equivalent matched on output voltage and current, control voltage, switching mode, isolation and footprint, or an alternative approach such as a form-factor change or a circuit-level redesign. Manufacturers sometimes publish transition guides, but they do not always exist, and final approval of any substitute belongs to your engineering team.

    Part discontinued, obsolete or hard to find?

    WIN SOURCE is a global independent distributor of electronic components, supporting component supply, shortage sourcing, lifecycle management and alternative solutions. Visual inspection, non-destructive testing and electrical testing are applied according to material risk, customer requirements and the applicable quality process, and orders are covered by the published return policy and a 3-year warranty on eligible components.

    Stock and pricing are updated daily — search a part number or contact us for current availability, lead time and a quote.

    Browse Solid State Relays  Upload a BOM / RFQ

    © 2026 Win Source Electronics. All rights reserved. This content is protected by copyright and may not be reproduced, distributed, transmitted, cached, or otherwise used without the prior written permission of Win Source Electronics.