1 … 273 274 275 276 277 … 364 2750 / 3635 POSTS

What are the benefits of linear drives?

* Question What are the benefits of linear drives? * Answer The benefits of linear drivers include: 1 avoiding the use of complex, expensive [...]

What is the development trend of the inverter?

* Question What is the development trend of the inverter? * Answer AC frequency conversion speed regulation technology is an effective way t [...]

Precautions when using transistors

* Question Precautions when using transistors * Answer If a piece of soldering piece is attached to the bolt, the circuit lead is soldered t [...]

What are the modules for the audio mixer?

* Question What are the modules for the audio mixer? * Answer (1) Headphone Mixer (2) Speaker Mixer (3) Mono Mixer (4) Mixer Output In [...]

What are the characteristics of semiconductor pressure sensors?

* Question What are the characteristics of semiconductor pressure sensors? * Answer Small size, high precision, low cost, good responsivenes [...]

What is a hardware description language?

* Question What is a hardware description language? * Answer The Hardware Description Language (HDL) is the language for electronic system h [...]

What is data online analysis processing?

* Question What is data online analysis processing? * Answer The English name of the online data processing and processing: OLAP, the full n [...]

What are the internal photoelectric effects that can be divided into several categories?

* Question What are the internal photoelectric effects that can be divided into several categories? * Answer 1 Photoconductive effect.Under [...]

What are the main technical characteristics of the T6321A?

* Question What are the main technical characteristics of the T6321A? * Answer 1 constant current output is 350mA; 2 input DC voltage rang [...]

What is the structure and principle of the vane air flow sensor?

* Question What is the structure and principle of the vane air flow sensor? * Answer The vane air flow sensor is also known as a vane or fla [...]
1 … 273 274 275 276 277 … 364 2750 / 3635 POSTS